STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Problem with video widget and FrontendApplication

On a custom screen which contains a VideoWidget, I added a button that calls a callback to go back to another screen. I switch the screen as it's suggested from ST by calling static_cast<FrontendApplication*>(Application::getInstance())->gotoHomeScre...

BDELI.2 by Associate II
  • 1818 Views
  • 3 replies
  • 0 kudos

Problems with Scrollable Container and text

Hello everyone :) I've got some problems with the Scrollable Container. I created a small application based on the "Scrollable Container example". If I scroll the text, there are some issues. There is a delay between scrolling and the updated display...

MWetter by Associate III
  • 2823 Views
  • 4 replies
  • 0 kudos

Simulator doesn't compile

   When starting Simulator it always fails even if I start completly fresh new project: I get the same result:In file included from C:/TouchGFX/4.16.1/env/MinGW/lib/gcc/i686-w64-mingw32/7.3.0/include/c++/bits/stl_algobase.h:66:0, ...

0693W00000HrXzVQAV.png
manto.1 by Senior
  • 1773 Views
  • 5 replies
  • 0 kudos

Resolved! Software problem

Hi there|I start to wrote my tiny first application with touchgfc and STM32G071 nucleo i just put one button with label . I want control a led. my problem is when i touch the button on the display nothingh append i try to put one breakpoint in the...

0693W00000HrTLbQAN.png 0693W00000HrTLRQA3.png 0693W00000HrTLMQA3.png 0693W00000HrTLHQA3.png
SGian.1 by Senior
  • 2155 Views
  • 4 replies
  • 0 kudos

Resolved! How can I chage the TextArea?

Hi, I used the STM32F429Zi discovery board.​So, I try to change the value to TextArea, but It's not work.​I created a project with reference to the following site.​https://www.youtube.com/watch?v=4xxkN9h0HYI*. Use the TouchGTX and make UI*. Make hand...

0693W00000HrVefQAF.jpg 0693W00000HrVfiQAF.png 0693W00000HrVg7QAF.png 0693W00000HrVgbQAF.png
지한.1 by Associate II
  • 1842 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.