2022-01-14 12:32 AM
Hello everyone :)
I've got some problems with the Scrollable Container. I created a small application based on the "Scrollable Container example". If I scroll the text, there are some issues. There is a delay between scrolling and the updated display of the text. It does not run smoothly.
It does not matter if I enable scrolling vertical, horizontal or both.
But on the other screen is a (horizontal) Scroll List with 12 Icons. There is no problem.
It works perfectly. If anyone has a hint for me....
Thank you very much
2022-01-14 12:56 AM
Hi,
Could you provide more information or images on what issue you are facing with texts (maybe your project or code as well) ? What are you trying to do exactly ? How did you implement it ? What version of TouchGFX are you using ?
/Romain
2022-01-14 1:06 AM
Oh sorry I forgot some things :)
Our evaluation board is the STM32H7B3-dk with a custom display (5", 800x480).
We use FreeRTOS, external SDRAM.
It works perfectly. There is just this one problem.
We used TouchGFX V4.15 with CubeMX 6.3 and CubeIDE1.5.1.
2022-01-14 1:17 AM
I had a weird issues with H7 too. It was memory performance issues, and finally they were solved with correct CM7 memory protection (caching and buffering). Check STM guidelines AN4861 "Creating a graphical application with LTDC" / section 4.6 Special recommendations for Cortex-M7 (STM32F7/H7) mentioned by @SofLit reply to my problem: https://community.st.com/s/question/0D73W000001N9NY/detail?s1oid=00Db0000000YtG6&s1nid=0DB0X000000DYbd&emkind=chatterCommentNotification&s1uid=0050X000007vlPS&emtm=1640338065814
2022-01-14 1:24 AM
Thank you. I'll check it :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.