STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Cyrillic language on touch gxf on stm32f7

Hi community.. I am doing an application to display some text in a display 5 inches.. I am using stm32cubeide and touch gfx.. They are asking me to support the cyrillic and hebrew language.When i Set the text on the gui and i try to watch it statical...

_legacyfs_online_stmicro_images_0693W00000biVUNQA2.png
SGasp.1 by Senior
  • 2384 Views
  • 5 replies
  • 0 kudos

Translations.rb never finishes

I want to export texts.xml to .xlsx with running the following comand ruby translations.rb export texts.xml texts.xlsxthe problem is that it never finishes I left it running more than 30 minutes. Text.xml was generated by TouchGFX 4.21.2.This was wo...

manto.1 by Senior
  • 2659 Views
  • 3 replies
  • 1 kudos

Resolved! Touchgfx Designer is not opening in the computer.

 last time also this problem was occured so I installed it again after that it run for some days now again the problem has occured. When I open Touchgfx one msg comeSorry - something unexpected has happened which caused an error to occur in the Desig...

MPath.4 by Associate II
  • 15630 Views
  • 25 replies
  • 0 kudos

stm32f429 discovery를 사용하고 있는�?� touchgfx 를 사용해서 프로그램 다운로드하면 정�? 입니다.

Hello, I am using stm32f429 discovery, and if I download the program using touchgfx, it is normal.By the way, HAL_Init(); MX_GPIO_Init(); //MX_I2C3_Init(); MX_SPI5_Init();MX_FMC_Init(); MX_LTDC_Init(); MX_DMA2D_Init();....If you remove only the touch...

Nhor.1 by Associate II
  • 1680 Views
  • 1 replies
  • 0 kudos

GFXMMU Vertical Flip Display

Hi, I am looking into processor based ways to flip the display, using a STM32L4R9. My display can handle horizontal pixel flip, but unfortunately not vertical so I want to see if I can do that without too much overhead in the processor.@Martin KJELDS...

RBurg.2 by Associate II
  • 1918 Views
  • 1 replies
  • 0 kudos

Resolved! how i can add my soucre file to TOUCH GFX ??

i am having a problem trying to add a source code to my project, even though CUBE IDE already added it but the source codes of TOUCH GFX are not receiving, i see people using Makefile to add it but i am having trouble towel when using it.I would be v...

_legacyfs_online_stmicro_images_0693W00000bjTSgQAM.png _legacyfs_online_stmicro_images_0693W00000bjTSlQAM.png
OWLchan by Associate III
  • 2741 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.