STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

display mipi - sending a dummy black portion

Hi programmers !I'm trying to work whit AVD-TT78QT-NN-005-S mipi display (1280x400 pixel) and STM32 U5A9J-DK board.This display needs a black portion of screen to visualize the image correct: (from datasheet)Obviously the screen in Touchgfx designer ...

vitom_0-1690788232628.png
vitom by Associate II
  • 1158 Views
  • 0 replies
  • 0 kudos

Resolved! ERROR IN TOUCH GFX 4.21.4

i am having problem when i try to use demo or create a project, these errors keep repeating even when i restart the app i have uninstalled 4.21.3 and installed the latest version but it keeps crashing.​Did I skip any steps during code generation or i...

_legacyfs_online_stmicro_images_0693W00000bipKmQAI.png _legacyfs_online_stmicro_images_0693W00000bin0uQAA.png _legacyfs_online_stmicro_images_0693W00000bimzmQAA.png
OWLchan by Associate III
  • 6704 Views
  • 11 replies
  • 1 kudos

Calibri font problem

Hello, I use STM32F746 and 800x480 TFT display and I use Calibri fonts but some calibri fonts cannot be shown correctly. I tried all texts with BPP8, BPP4, BPP1, but nothing is changed. How can I solve this?

Epamuk by Associate III
  • 4409 Views
  • 5 replies
  • 0 kudos

TouchGFX calls HAL_Delay in ISR

Hi,In TouchGFXHAL.cpp, HAL_DSI_EndOfRefreshCallback() contains HAL_Delay(). Meantime it is called from HAL_DSI_IRQHandler(). Can it be avoided?The code is generated with TouchGFX Designer 4.22.0 for STM32H747I-DISCO.The generated file is attached.

ERROR by Senior
  • 2835 Views
  • 3 replies
  • 0 kudos

snprintf on wildcard only once

Hi friends, I have this problem:static uint16_t txt[10];Unicode::snprintfFloat(txt,6U,"%0.2f",functionGetFloat());Unicode::snprintf( TextIndicatorBuffer,TEXTINDICATOR_SIZE,"%s %s",TypedText(T_STATEPRODUCTMANAGERWC5).getText(),txt);TextIndicator.setWi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.