STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! DMA2D signals transfer completion too soon?

I used STM32CubeIDE to create the LCD_DSI_CmdMode_DoubleBuffer for the STM32F769I-DISCOVERY board. It works fine, but I made some modifications to just draw a rectangle:    if 1 BSP_LCD_SetTextColor(LCD_COLOR_RED); BSP_LCD_FillRect(0, 0, 800, 240...

20230815_080956.jpg
_Nick by Associate
  • 1833 Views
  • 1 replies
  • 1 kudos

Resolved! Touchgfx and user input

Hi since I am very new to touchgfx this is probably a wrong or already answered question. How can someone has a user edited text line or text area with a virtual keyboard? I mean to have a text input widget that user selects it and a keyboard opens o...

Kyrpav by Associate III
  • 3100 Views
  • 3 replies
  • 1 kudos

touchgfx led backlight control

I have bought a riverdi display RVT50HQTNWC00, i want to know if at the backlight pins that the typical is 12volts i can connect a 12vdc power adapter for test or i need to use a led driver like TPS61169.

Kyrpav by Associate III
  • 4279 Views
  • 8 replies
  • 4 kudos

Resolved! TouchGFX: TouchGFX_Task Only Called Once

Hello,I am running on the STM32H725AGI6 on a custom board. I am trying to use the TouchGFX GUI with the LTDC interface (RGB565). I am trying to run a firmware that I had previously working on another of the H7 series (STM32H7B3IIT6). The hardware is ...

KMew_0-1691086518290.png
KMew by Senior III
  • 2719 Views
  • 3 replies
  • 0 kudos

Resolved! Horrible displayed content quality

Hello, I am using STM32H7 with a circular display (driver HX8363-A). One of the problems that I seems to have is that although on the TouchGFX software the content looks nice, the moment I display that same content on the physical display, it looks h...

montea by Associate II
  • 3614 Views
  • 3 replies
  • 2 kudos

Cube MX not generates lockDMAToFrontPorch(true);

Hello!I have old project. It has file TouchGFXGeneratedHAL.cpp, where I can see codevoid TouchGFXGeneratedHAL::initialize() { HAL::initialize();   registerEventListener(*(Application::getInstance())); enableLCDControllerInterrupt(); e...

EEuge by Senior
  • 1779 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.