2023-08-07 2:02 AM
Hi,
I am trying to make a relay driver with STM32H750DB-K, so I could switch the relays with toggle buttons on display, but I have a difficulty writing on digital pins.
When I don't generate code from TouchGFX (so starting from scratch) and just write on output pin E3 calling the function HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_SET); in while function of main.c the voltage on pin E3 is set to 3.3V as expected. But when I generate a simple code with TouchGFX (just a toggle button) and write function HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_SET); in while function of main.c (which is in TouchGFX folder) the voltage on pin E3 is 0V. I tried this on several pins, but it is always the same.
Is there something obvious that I am missing? Does anyone know the solution to this problem?
2023-08-07 2:15 AM
Generic codes can access the entire Port, this way despite momentarily having the state change in the HAL_GPIO_WritePin() instruction right after the display routines can be accessing the port that was controlled via HAL_GPIO_WritePin().
So that this type of problem does not occur when accessing the port, it is necessary to use a mask so that only the desired pins (bits) are modified.
uint32 target_reg = GPIOA->ODR; uint32 mask = (1<<5); // mask = 0x00000020 target_reg = target_reg | mask;
uint32 target_reg = GPIOA->ODR; uint32 mask = ~(1<<5); // mask = 0xFFFFFFDF target_reg = target_reg & mask;
2023-08-07 2:25 AM
I don't know if it can help in your case, but I found these videos about advanced debugging:
https://youtube.com/playlist?list=PLnMKNibPkDnEDEsV7IBXNvg7oNn3MfRd6
2023-08-14 2:10 AM
Perhaps the GPIO you try is later reconfigurated to be input or an alternate function.
Also check if \TouchGFX\target\TouchGFXGPIO.cpp happends to use your GPIO.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.