STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

QSPI XIP with TouchGFX

Our STM32L4S7 project is consuming internal flash much faster than we expected despite the fact that we've taken steps to move as many assets into external flash as we can, including SVG images.Our next approach is to see if we can split the TouchGFX...

ikendal by Associate
  • 1543 Views
  • 1 replies
  • 0 kudos

Container caching question

Hello,I would like to improve the performance of a scrollable container by caching its sub-containers.My framebuffer is in ARGB2222 mode.My current problem is that I always get a Hardault for unaligned access even if my framebuffer is in a MPU region...

i2399 by Associate III
  • 1422 Views
  • 1 replies
  • 0 kudos

Mix and Merge screens outside TouchGFX

 In TouchGFX online docs there is a Tip that I think it would be very interesting going deeper into.Are there examples? Someone tried this way? "Code StructureTIPOf course you do not need to use any features of the code generated by TouchGFX Designer...

Draw transparent rectangles

Hi there. I'm trying to figure out how to draw/fill rectangle with transparency. I can fill opaque rectangles without issues. I am using `stm32h750`, 320x240 ILI9341 LCD which supports RGB565 buffers. Below is the code that kinda works, but it genera...

brbrr by Associate II
  • 4654 Views
  • 7 replies
  • 0 kudos

Implementing my library

Hello, I am having problems adding my library to my project. I added the .h file to Core/Inc and my .c file to Core/Src. I included the .h in Model.cpp since that is where I want to use it. I can use the definitions that are in my header file but not...

MexiAxel by Associate II
  • 3164 Views
  • 6 replies
  • 0 kudos

Resolved! Object reference not set to an instance of an object error when trying to create Button Example

Hello,I have downloaded the latest version,4.22.1 of Touch GFX and selected the Button Example.When I tried to create the project Touch GFX prompted  "Object reference not set to an instance of an object error"Please see the log file attached. Mainly...

Kutlu by Associate II
  • 2399 Views
  • 1 replies
  • 1 kudos

Resolved! TouchGFX generator, no active the touch

I can configurate the touchGFX configurator with the stm32f746, i can open the .part and designer some figures and bottoms, these yes appears in the LCD, i use the hardware stm32f746 discoveryboard. But i no can active the function of the touch, have...

RMasi.19 by Associate II
  • 5446 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.