STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! What causes an "Invalid project path: Missing project folder or file: \PROJECT_NAME\GRAPHICS for Source path"

This is a warning listed under the "Problems" tab in STM32CubeIDE (1.1.0). I am seeing some strange behavior and am wondering if this is the cause.The strange behavior I am seeing is that often when I change something in the TouchGFX Designer and cli...

scottSD by Lead
  • 14042 Views
  • 17 replies
  • 1 kudos

Resolved! TouchGFX 4.16.1 Hardfaults when D-Cache is enable

Hi, I Have a custom board with stm32h743... I design a graph page with touchGFX and when D-cache is enable, system detect some hard faults specifically when I touch a button to change screens, some times it works and some times not, When I disable D-...

MHaji.1 by Senior
  • 2114 Views
  • 4 replies
  • 0 kudos

Resolved! TouchGFX color and other defines in designer.

Hi, maybe i ask this some years ago, but still not resolved. In designer now cant create defines list for use instead constant numbers. Then can be quickly managed all objects.Now for example i have designs with 150 labels and set some level of white...

MM..1 by Chief III
  • 4209 Views
  • 11 replies
  • 2 kudos

Resolved! Qrcode is not interpretable

Hi everybody,I'm trying to implement into a custom board, the dynamic Qrcode generation algorithm.I'm using touchgfx 4.23.0, an SPI display with partial buffer strategy.I would like to draw the string "https://support.touchgfx.com" . Display seem to ...

1708724847894.jpg 1708725457522.jpg
MPast.1 by Senior II
  • 25107 Views
  • 18 replies
  • 3 kudos

Resolved! how to get a tpa version?

I am working on custom display board. created project using touchGFX I would like to know to how to confirm what is the tpa version touchGfx used to create this project.any interface to get tpa version or BOM file which includes all package version. ...

jsalg.1 by Associate III
  • 3256 Views
  • 4 replies
  • 2 kudos

Resolved! scrollable container

Hi,i have a scrollable container with some objects inside:on the left and right i have these images:       i need to hide the images images on left and right border according to scroll position and number of objects:if objects are <= 6 hide left and ...

ToniT_0-1709043288012.png ToniT_1-1709043818917.png ToniT_2-1709043862841.png
ToniT by Associate II
  • 2316 Views
  • 2 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.