STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Missing needles in TouchGFX Designer-4.23.0

Hello, I have made a simple application with STM32G071RB_NUCLEO and an X-NUCLEO-GFX01M2 I TouchGFX. The problem is that the needle in the Gauge or the hands in the analogue clock are not displayed. When I look at Memory Details in STM32CubeIDE I can ...

amigafan by Associate III
  • 7981 Views
  • 6 replies
  • 2 kudos

Resolved! Are there any plans to make responsive UI on TouchGFX?

I've been using LVGL for a while and I must say, their implementation (much based on CSS styles) is good to make responsive designs that scale based on screen size. Their concept is very simple, every object have a flex property that can be enabled. ...

Dolence by Associate III
  • 2016 Views
  • 1 replies
  • 0 kudos

Resolved! TouchGFX Designer with TrustZone-enabled U5

Hi,seems like TouchGFX Designer is unable to create a compilable folder structure for TrustZone-enabled U5 projects. So far the workaround is to use a separate non-TrustZone project and then manually sync all the changes made by TouchGFX Designer bac...

bear2023R by Associate III
  • 4260 Views
  • 4 replies
  • 1 kudos

Resolved! Random color pixel problem

Hi everyone. I set a flag, and checked it in handleTickEvent of any page. I give new location to images when the flag is set. I have a problem in this point. Sometimes(approximately 1/50 flag set), i see random color on some pixels. I research this p...

IMG_20240302_174305.jpg IMG_20240302_174423.jpg IMG_20240302_174815.jpg IMG_20240302_180001.jpg
erkanc by Associate III
  • 3090 Views
  • 4 replies
  • 0 kudos

X-CUBE-TOUCHGFX 4.23.1 is out!

TouchGFX 4.23.1 is now out. Please follow this link to download it. 4.23.1 Release details: Release date: January 22nd, 2024 New TouchGFX Designer Features: Bugfixes in TouchGFX Designer: Fixed TextArea lineheight in canvas not matching with rende...

how to save values in non-volatile memory qspi

Hellohow to save (int, float...) values, in non-volatile memory on a riverdi RVT70HSSFWCA0 screen. It has an external qspi flash. Can you give me some simple basic examples or a demo file? I think we should use HAL FLASH? and the code should be put i...

NicoEFI by Associate III
  • 4148 Views
  • 8 replies
  • 4 kudos

STM32H7B3I-DK screen just staying white

I've been trying to test out the screen on the board I just got. I can get the examples to work fine, but even if I copy the values over to my project, nothing shows (the project is just a blank project generated by the IDE). Pretty new to display st...

0693W00000FBHA5QAP.png 0693W00000FBHA0QAP.png
LRusi.1 by Associate
  • 2585 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.