STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Flash screen of STM32H747I-DISCO

PART# STM32H747I-DISCO (Mouser S/O 935751) We have a customer tried the demo program on ST website, ​./en.STM32H747I-DISCO_demo/STM32H747I-DISCO_demo"Three example programs based on TouchGFX�?STemWin�?EmbeddedWizard, open a random folder, use STM32Cu...

LSong.11 by Associate II
  • 11548 Views
  • 7 replies
  • 0 kudos

Resolved! How to add custom container during runtime

Hello everyone, I am trying to improve my skills with TouchGFX. I want to add dynamically a custom container at my current screen during runtime. Is there a method to do it without using a container widget? I don't want to put my custom container in ...

FCola1_4-1708679383016.png Catturast3.PNG Catturascreen.PNG FCola1_0-1708679065472.png
FCola.1 by Associate III
  • 2171 Views
  • 1 replies
  • 1 kudos

Resolved! TouchGFX on custom board

I am working on touchGFX on custom board where I am creating my project in CubeIDE.I have integrated the touchGFX in .ioc file but when I try to compile the code in TouchGFX designer I get following error  Post Generate Target    touchgfx update_proj...

AS.19 by Associate II
  • 3852 Views
  • 6 replies
  • 0 kudos

Resolved! drawed CircleCheckBox

Hello,I needed to create some drawed ones elements. My request was the ability to change the color on the fly, the ability to set the day and night mode and possibly change the dimensions.I am sending here the first working version without setting th...

jnCircleCheckBoxA.png
JNova.0 by Associate III
  • 2640 Views
  • 3 replies
  • 1 kudos

Resolved! low costs Touch gfx gui freezes

Hi.I started a small project using a custom board with STM32G0B0, SPI flash and 3.5 inch ili9488 LCD, communicating via SPI using the TE pin, without RTOS. Everything loads fine and quite fast, but after 5-40 seconds the uC freezes. Especially when c...

Jin454 by Associate III
  • 6248 Views
  • 7 replies
  • 2 kudos

How to display ADC data in 12 graphs in real-time

Dear all,I am working on a project using STM32F750 (custom board), a 7 inch TFT touch LCD (using LTDC), and FreeRTOS v1.I have 12 analog signals (ECG signals) captured by ADC every 1ms.I want to plot them (real-time) on 12 different graphs on LCD.My ...

hmasg by Associate
  • 2514 Views
  • 1 replies
  • 3 kudos

How to draw a dynamic picture at runtime?

I’m using STM32CubeIDE 1.2.1 and TouchGFX 4.13.0 with STM32F746G-DISC0 kit.I would like to calculate an image at runtime and then display it. Is there a manual or something similar? I have tried the AnimationStorage, unfortunately getAnimationStorage...

DMeix.1 by Associate II
  • 7375 Views
  • 12 replies
  • 0 kudos

TouchGFX with stm32f412g-disco

Good morning,I bought an stm32f412g-disco board but it's impossible to program the screen with a TOUCHGFX application.I'm using TOUCHGFX Designer 4.23 and stm32cubef4-v1-28I created a project directly from TOUCHGFX Designer for the F412G-disco board....

20231215_080853.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.