2024-10-28 5:44 PM
Hi there Touchgfx team,
Touchgfx can not run simulator or generate code on my Win11 laptop. I found out that touchgfx needed administrator access to have those function in Win11, but Win10 not. Because my laptop is for working and provided by my company, I don't have administrator access in Win11.
Is there any plan to fix this issue?
2024-10-28 8:31 PM - edited 2024-10-28 8:32 PM
>>Is there any plan to fix this issue?
If you're working on this for work, this would seem to fall squarely on your IT staff
Perhaps you can VirtualBox a Win10 instance? Or get issued a Win10 desktop or laptop
2024-10-28 10:12 PM
Hi @Tesla DeLorean ,
Thanks for your suggestion.
I have asked for help to the IT staff. And his answer is impossible to give the administrator access to me. If touchgfx will not fix this, I have to downgrade my laptop to Win10.
2024-10-29 5:53 AM
Hello @Chand446209 ,
Could you show me what's the exact message ?
Best regards,
2024-10-29 7:45 PM
Hello @LouisB ,
I opened a project which can generate code and run simulator with no issue in Win10. But it is failed in my Win11.
I attached two pictures for the generate code log and run simulator log. If I run touchgfx with the administrator access, both are success.
2024-10-31 7:09 AM
Hello @Chand446209,
which version of windows 11 are you using ?
2024-11-03 7:26 PM
Hello @LouisB ,
Please check my Win11 version below.
Edition Windows 11 Pro
Version 23H2
Installed on 4/10/2024
OS build 22631.3880
Experience Windows Feature Experience Pack 1000.22700.1020.0
2024-11-07 7:19 PM
2024-11-19 6:21 AM
Hello @Chand446209 ,
You are sure you have the exact same rights and configuration on the win 10 and 11 ? I looks related to your win 11 setup.
Best regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.