2020-04-02 1:44 PM
Hello, does anyone know how to programmatically calculate a CRC with a polynomial length of 8 and 16 bits? The algorithm described in AN4187 only works with a 32-bit polynomial. Here are the results:
IN_REVERSE_NONE, OUT_REVERSE_NONE, POLY_32B - 0xe8bccd9a
IN_REVERSE_NONE, OUT_REVERSE_NONE, POLY_16B - 0x3852
IN_REVERSE_NONE, OUT_REVERSE_NONE, POLY_8B - 0x26
IN_REVERSE_NONE, OUT_REVERSE_NONE, POLY_7B - 0x60
IN_REVERSE_NONE, OUT_REVERSE_BIT, POLY_32B - 0xaa45c417
IN_REVERSE_NONE, OUT_REVERSE_BIT, POLY_16B - 0x6e52
IN_REVERSE_NONE, OUT_REVERSE_BIT, POLY_8B - 0xfd
IN_REVERSE_NONE, OUT_REVERSE_BIT, POLY_7B - 0x5d
IN_REVERSE_BYTE, OUT_REVERSE_NONE, POLY_32B - 0x790ac5f0
IN_REVERSE_BYTE, OUT_REVERSE_NONE, POLY_16B - 0x1ae2
IN_REVERSE_BYTE, OUT_REVERSE_NONE, POLY_8B - 0x69
IN_REVERSE_BYTE, OUT_REVERSE_NONE, POLY_7B - 0x7
IN_REVERSE_BYTE, OUT_REVERSE_BIT, POLY_32B - 0x8794adc5
IN_REVERSE_BYTE, OUT_REVERSE_BIT, POLY_16B - 0x752a
IN_REVERSE_BYTE, OUT_REVERSE_BIT, POLY_8B - 0x70
IN_REVERSE_BYTE, OUT_REVERSE_BIT, POLY_7B - 0x77
IN_REVERSE_HALFWORD, OUT_REVERSE_NONE, POLY_32B - 0x4aaf6021
IN_REVERSE_HALFWORD, OUT_REVERSE_NONE, POLY_16B - 0x867c
IN_REVERSE_HALFWORD, OUT_REVERSE_NONE, POLY_8B - 0xdc
IN_REVERSE_HALFWORD, OUT_REVERSE_NONE, POLY_7B - 0x3b
IN_REVERSE_HALFWORD, OUT_REVERSE_BIT, POLY_32B - 0x71122de7
IN_REVERSE_HALFWORD, OUT_REVERSE_BIT, POLY_16B - 0x4c72
IN_REVERSE_HALFWORD, OUT_REVERSE_BIT, POLY_8B - 0x53
IN_REVERSE_HALFWORD, OUT_REVERSE_BIT, POLY_7B - 0x39
IN_REVERSE_WORD, OUT_REVERSE_NONE, POLY_32B - 0x3ec460e8
IN_REVERSE_WORD, OUT_REVERSE_NONE, POLY_16B - 0x655
IN_REVERSE_WORD, OUT_REVERSE_NONE, POLY_8B - 0xd8
IN_REVERSE_WORD, OUT_REVERSE_NONE, POLY_7B - 0x3
IN_REVERSE_WORD, OUT_REVERSE_BIT, POLY_32B - 0xd2eef894
IN_REVERSE_WORD, OUT_REVERSE_BIT, POLY_16B - 0xc88d
IN_REVERSE_WORD, OUT_REVERSE_BIT, POLY_8B - 0xbd
IN_REVERSE_WORD, OUT_REVERSE_BIT, POLY_7B - 0x1e
Software CRC32 - 0xe8bccd9a
Software CRC16 - 0xf6f4
Software CRC8 - 0xea
CRC calculate function:
TYPE: CRC32 --> uint32_t, CRC16 --> uint16_t, CRC8 --> uint8_t
TYPE CRC_CalculateType(TYPE data)
{
const TYPE polynom = LL_CRC_GetPolynomialCoef(CRC);
const TYPE max_bits = sizeof(data) * 8;
const TYPE mask = (TYPE ) 1 << (max_bits - 1);
TYPE crc = LL_CRC_GetInitialData(CRC) ^ data;
for(int i = 0; i < max_bits; ++i)
{
crc = (crc & mask) \
? (crc << 1 ^ polynom) \
: (crc << 1);
}
return crc;
}
2020-04-02 3:02 PM
>> The algorithm described in AN4187 only works with a 32-bit
Honestly seems more general than that. But does make some assumptions about bit shift direction, and data lsb/msb
Some of the STM32 products only support 32-bit in hardware, and have some novel shift, word length, and endian usage.
>>does anyone know how to programmatically calculate a CRC with a polynomial length of 8 and 16 bits?
Yes, I've built a number of HW and SW implementations. Posted several table driven methods to the forum.
2020-04-02 3:13 PM
Can you attach the links?
2020-04-02 3:23 PM
I'm stuck using the site search like everyone else...
Here's one https://community.st.com/s/question/0D50X0000CDmAkpSQF/calculate-crc8
I'd imagine if you dig you can find others.
The code you posted presupposes the data length is the same as the CRC, most cases people feed in bytes, there endian ordering becomes an issue. It also shifts left and assumes the data comes msb first.
What polynomial, size and shift direction are you looking for? Provide the specification, and example data.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.