STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CRC calculation using srec_cat

I am using STM32F207. The project that im working on will later on will be used by a bootloader. I am, therefore, trying to add crc information in the hex file so that bootloader will be able to validate its correctness.I am using srec_cat to calcula...

Ashei.8 by Associate II
  • 12455 Views
  • 9 replies
  • 0 kudos

STM32G4 SBSFU do not display Welcome screen

I tried to step-by-step execution based on UM2262. But I could not get SBSFU welcome screen display (Fig24). My SBSFU display below.[SBOOT] Flash Configuration KO: Dual bank mode activated. STOP![SBOOT] Security issue: execution stopped!My step-by-st...

NR-A Comm by Associate II
  • 4391 Views
  • 6 replies
  • 0 kudos

Software CRC with a polynomial length of 8 and 16 bits

Hello, does anyone know how to programmatically calculate a CRC with a polynomial length of 8 and 16 bits? The algorithm described in AN4187 only works with a 32-bit polynomial. Here are the results:IN_REVERSE_NONE, OUT_REVERSE_NONE, POLY_32B - 0xe8b...

I have enabled level 1 rop in stm32f030c8, now my code is not working in device and m not able to load fresh code or debuge it using attolics true studio.

here's my code for RDPprotection:void Flash_SetRDPLevel(uint8_t ReadProtectLevel) //level 1 (0xBB){ uint32_t tmp_reg; Unlock(); OB_unlock();  /* Read RDP level bits */  tmp_reg = (FLASH->OBR & (FLASH_OBR_RDPRT1 | FLASH_OBR_RDPRT2));  //if (tmp_re...

shikha by Associate II
  • 2032 Views
  • 3 replies
  • 0 kudos

Resolved! Calculate CRC-8

Hello,I need to know how to calculate CRC-8 of input data.I have a binary stream like (12586966 Dec or 0XC00FD6) and CRC-8(22 DEC, 0x16). Based on 0x97 polynomial how I can calculate my input binary stream CRC-8?Thanks

parisa by Senior
  • 20970 Views
  • 6 replies
  • 0 kudos

Resolved! Board does not boot after readout protection enabled.

I have a project based on an Stm32F767. If I load the hex file and then manually enable readout protection to level 1 with the STLinkV2 utility, the board fails to begin to execute code after reset. Why? What is the correct way to use this feature?

CSeto.1 by Associate
  • 1826 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.