STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Decoder of ASN.1 format to read RSA public key

Hello, I am using the STM32 Cryptolib. I need to get the modulus and exponent of RSA public key from a .pub or .pem files. After decoded from base64 I need to decode the DER format (in ASN.1 format). Has anyone any suggestion of which libray may I us...

lukin by Associate III
  • 8320 Views
  • 9 replies
  • 1 kudos

Resolved! Tamper: not able to update into the seed registers

Hi all,I'm trying to implement Active Tamper in STM32U585 controller, im trying to generate the SEED, the Seed is getting generated, but the SEED is not getting updated in the SEED reg of tamper, i'm attaching the code and seed values generated for r...

meghasb_0-1700136839457.png meghasb_1-1700136874433.png meghasb_2-1700137019153.png
meghasb by Senior
  • 2162 Views
  • 3 replies
  • 0 kudos

Resolved! cannot launch UserAPP after SBSFU

Hi, I am a beginner in SBSFU.STM32L4S7ZIT6STM32CUBEIDE Version: 1.12.0STM32CUBEProgrammer v 2.13.0 (for download SBSFU and full chip erase)Tera Term v 4.106When run SBSFU, I can get EXECUTE USER FIRMWARE at end, but cannot run UserAPP.if reset SBSFU,...

alyssa_0-1699955016076.png alyssa_3-1699956507644.png alyssa_4-1699957019484.png alyssa_2-1699956302724.png
alyssa by Associate III
  • 2465 Views
  • 2 replies
  • 0 kudos

Resolved! Generate key pair geneartion

 Am using Nucleo-STM32H573 Board.   i wanted to generate a pair of public and private keys.  Guide me

RKOAS by Associate II
  • 2340 Views
  • 1 replies
  • 0 kudos

External PSRAM not working when using SBSFU

Hi,In my application using stm32l496zgt6 I'm using DCMI to capture Image and storing image Data in External PSRAM  , this code works fine, Problem is whenever integrating this piece of code with application using SBSFU, As soon as MX_FMC_Init(); func...

RSA Pair Key generation on STM32L496

Hello,I am working on STM32L496, that does not have an AES hardware encryption, and i wanted to generate a pair of RSA Keys, public and private keys.I wonder if i can use mbedTLS or any library to do so or not?If i can do it, is there any example or ...

aybood by Associate
  • 1610 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.