2023-11-28 6:28 AM - edited 2023-11-28 7:13 AM
Hi,
I'm trying to encrypt and decrypt in my device, running on a STM32H753, using AES ECB.
I'm initializing crypto like this:
hcryp.Instance = CRYP;
hcryp.Init.DataType = CRYP_DATATYPE_8B;
hcryp.Init.KeySize = CRYP_KEYSIZE_256B;
hcryp.Init.DataWidthUnit = CRYP_DATAWIDTHUNIT_BYTE;
hcryp.Init.pKey = AESKey256;
hcryp.Init.Algorithm = CRYP_AES_ECB;
/* Enable CRYP clock */
__HAL_RCC_CRYP_CLK_ENABLE();
/* Force the CRYP Peripheral Clock Reset */
__HAL_RCC_CRYP_FORCE_RESET();
/* Release the CRYP Peripheral Clock Reset */
__HAL_RCC_CRYP_RELEASE_RESET();
MODIFY_REG(hcryp->Instance->CR, CRYP_CR_DATATYPE | CRYP_CR_KEYSIZE | CRYP_CR_ALGOMODE,
hcryp->Init.DataType | hcryp->Init.KeySize | hcryp->Init.Algorithm);
2023-11-28 8:32 AM
I've seen this post https://community.st.com/t5/stm32-mcus-security/how-to-enable-the-stm32h750vbt6-hw-crypto/td-p/165187 which seems to show the same problem. There, ST explains that there is a batch from 2020 with no cryptographic features.
From my side, it seems I have two different batches of microcontrollers:
1- STM32H753IIKb with date code 946 (2019 week 46?): these ones are working fine.
2- STM32h753IIKb with date code 133 (2021 week 33?): these ones not working, with registers in zero even after writing into them, as if clock was not initialized.
Did I just bump into another batch without crypto? how could I get a confirmation from ST?
2023-11-28 8:52 AM
Submit on Online Support Request via the ticket submission process. https://www.st.com/content/st_com/en/support/support-home.html
Alternatively talk directly with your local sales office, or FAE supporting your account.
As I recall Pavel provided a means to check if the unit is enabled, or not. Begin enabled or not is likely a final test fuse, but could be a mask-set metal layer. The parts could also be counterfeit, or mismarked. You should share the trace codes on the packaging or reels with ST privately.
2023-11-28 9:04 AM
Some of the other threads / links are borked..
This is the one with Pavel's code https://community.st.com/t5/stm32-mcus-security/stm32h750vbt6-access-crypt-registers-all-read-back-zero/td-p/204834
2023-11-28 11:14 AM
Dear @Tesla DeLorean ,
Thank you for the insight, @TVare.1 I confirm that we had in second half of 2020 a test program issue at our factories, during manufacturing, leading to cryptographic feature disabled (CRYP and HASH). In case these cryptographic features would be used in final application, functionality failure will be visible immediately (100% failure rate) as you have seen with 0x000..
We sent a Quality Alert to all of our customers/distributors at that time by December 2020 and then Issue is fixed at our Factories, To be very specific not all parts are impacted by few Lots at specific factory where date code is from 2020 Week 22 to 2020 Week 47 . 022 to 047 may be impacted.
In case customer application would require these specific cryptographic features and to avoid any customer manufacturing burden, ST recommends recalling all unused impacted material and will issue a return material acceptance (RMA) accordingly, so please to go in touch with your local distributor or ST sales Offices. Our customers not using theses features, they will not see such impact.
Now it seems your Date code is different and from 2021, we need to check it if coming from ST and may be the issue happened again but we are not aware of it so far.
Hope it is more clear now.
Ciao,
STOne-32.
2023-11-29 1:37 AM
Thanks all for the answers.
Indeed I checked Pavel's code in my main, and it is consistent with my description. In those devices from 2019 it works fine, but when used in 2021 uCs it returns false.
It happens both for HASH and CRYP, for which I adapted like this:
// Test if the STM32H7 crypto is actually working,
// so this is H7 variant with crypto (ex. H753 vs H743)
// Check that CR regster of HASH or CRYP holds written value
bool H7_hw_crypto_test()
{
// Test if HASH->CR is writable
__HAL_RCC_CRYP_CLK_ENABLE();
HAL_Delay(5);
CRYP->CR = 0;
__DSB();
CRYP->CR = 0x20; // set HASH_CR_DATATYPE=HASH_DATATYPE_8B
__DSB();
uint32_t u = CRYP->CR;
bool y = ((u & 0x30) == 0x20);
if (!y) {
__HAL_RCC_CRYP_CLK_DISABLE();
}
return y;
}I'll continue in private with @STOne-32 to check the trace codes. Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.