STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U585 DOES NOT RETURN TO RDP=0.

Hello,I've added the OEM2KEY AND OEM1KEY to the RDP Level 2 protection in order to perform the same steps as in the 'Getting started with STM32CubeU5 TFM application' for enabling Production Mode.Following the steps and executing the HARDENING.SH fil...

Istillaga_0-1713193265654.png

TFM SPI issue in custom board with STM32u585aii6q

Hi @Jocelyn RICARD Greetingswe are trying to run TFM example (with secure and non secure project) taken from GPIO_Toggle_TZEN Example and adding SPI communication in the non secure project on our custom board mounted with STM32U585aii6q controller SP...

PJose.4 by Senior
  • 6188 Views
  • 12 replies
  • 1 kudos

Resolved! PKA Modular Exponentiation not working as expected

Hello,I'm trying to figure out how to properly use STM32WB55 PKA registers for RSA key generation and encryption/decryption. I have chosen small (63 bit) primes for generating RSA private key, which worked perfectly. However, I am having trouble with...

PKryg.1 by Associate II
  • 3483 Views
  • 5 replies
  • 2 kudos

Support required with SBSFU Implementation on STM32WB55

Hello ST Community,I'm currently working on a project using the STM32WB55 MCU and am in the process of implementing Secure Boot and Secure Firmware Update (SBSFU) in my custom application. As part of this, I decided to test the existing 1_Image_SBSFU...

Sjain_0-1719740326469.png Sjain_1-1719740338555.png
Sjain by Associate III
  • 3847 Views
  • 5 replies
  • 0 kudos

Resolved! SBSFU example code

Hi ,i am using STM32L4R9 based dev board STLINK-V3MINIE and wanted to use SBSFU, used the example code STM32L432KC_Nucleo_1_image from the library and flashed the SECoreBIN followed by SBSFU and then the userAPP code, but while flashing userAPP ,i go...

Resolved! STM32F103VCT6 code read out protection

Hi,I have read datasheet of STM32F103VCT6, it does not mention anything about code read out protection. Does STM32F103VCT6 has this function? (a security function to protect STM32F103VCT6 from reverse engineering)Thank youDavid Kean 

ECC Signature Failure

Reference: STM32CubeExpansion_Crypto_V4..1.0, MCU: STM32G474REThe cmox_ecdsa_verify(...) function is failing with a fault code of 0x6c706, which is not contained within cmox_ecc_retvals.h header file. All arguments to the cmox_ecdsa_verify(...) funct...

rrooyen by Associate III
  • 14980 Views
  • 20 replies
  • 8 kudos

Resolved! Setting product state CLOSED without keys loaded

Hello,I have done a big mistake. I was testing a provisioning using the system bootloader. For that I have changed the provisioning batch files. As a result I have set the product state to closed, before the keys where loaded.  Now I can not connect ...

RomThi by Associate III
  • 2283 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.