STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-AZURE-H7 hw cryptographic acceleration

Hi Team,Is there roadmap for implementation hardware cryptography acceleration for NetX Secure using CRYP peripheral at STM32H7?I am using STM32H735@520MHz and I am not able achieve more than 800kBit/sec for HTTPs connection (TLS 1.2 TLS_RSA_WITH_AES...

JDosp.1 by Associate III
  • 11510 Views
  • 19 replies
  • 1 kudos

Resolved! STM32 cryptographic firmware ECDSA

Hi ST,     What tool generated the following data?Can you send me this tool? thanks. https://www.st.com/en/embedded-software/x-cube-cryptolib.htmlSTM32 cryptographic firmware library software expansion for STM32Cube. The path of the code is as follow...

Roger0x0000_1-1721790709207.png

SBSFU - Example Project NUCLEO-G474RE

I want to use SBSFU for a SW Update OTA Project , i try to compile the example project from SBSFU-Projects:  NUCLEO-G474RE_2_Images_SBSFUNUCLEO-G474RE_2_Images_SECoreBin (first, this project will be compile)NUCLEO-G474RE_2_Images_UserApp by try to co...

Resolved! STiRoT Provisioning of STM32H573 over SPI

Hi all,we are developing a product with the STM32H573. The idea is to use the STiRoT for secure firmware update. The MCU is connected to a Linux CPU via SPI. Now we plan to do the provisioning during the production using the Linux CPU that has a ethr...

RomThi by Associate III
  • 8622 Views
  • 12 replies
  • 1 kudos

STSAFE-A110 with mbedTLS and local envelope API

I'm using an STSAFE-A110 chip with SPL02 profile on a custom board and trying to get StSafeA_WrapLocalEnvelope() function working. I've already successfully paired my chip with my MCU/FW by writing the default host MAC key from the ST examples to the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.