STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to flash .sfi file to stm32h753 use HSM?

I got an error when downloading the .sfi file to STM32H753II using the STM32Programmer_CLI, my HSM version is V2AE.The error message is as follows: What its mean?V2AE cannot support STM32H753,and must use HSM_V1?or H753 cannot support SFI ?I’m a new ...

SONGTAOSI_0-1776998424623.jpeg

STM32H7 Cant Set PROT_AREA Option Bytes

Hello All,I have a certain STM32H7 that I can't erase sector 0 using STM32CubeProgrammer.I think it is because PROT_AREA_START1 and PROT_AREA_END1 are not correct. I am trying to get back to default values of PROT_AREA_START1 =0xFF (0x0800ff00)PROT_...

TCash.1 by Associate III
  • 3936 Views
  • 7 replies
  • 0 kudos

PQC Support on STM32U585 controller

Hi EveryoneRequesting clarification on one topic:Does STM32U585 have support for PQC algorithm with any software library that has been validated on the same controller, as there is a requirement for PCI PTS 7, that the device should support PQC Algor...

PJose.4 by Senior
  • 660 Views
  • 8 replies
  • 3 kudos

Resolved! Validating FW Image on NUCLEO-H753 SBSFU example

Left commented out SFU_NO_SWAP and defined ENABLE_IMAGE_STATE_HANDLING in app_sfu.h, but when trying to build SECoreBin and SBSFU errors appear:/Middlewares/ST/STM32_Secure_Engine/Core/se_fwimg.h:47:61: error: unknown type name 'SE_FwStateTypeDef'Is ...

lakins by Associate II
  • 288 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.