STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Cryptolibrary 4.x.x (cmox) RSA preallocated buffer

How do you know how big the preallocated static buffer should be when calling cmox_rsa_construct?Does this depend on the RSA key size that will be used?Does this depend on the Modular Exponentiation function that is selected (LOWMEM, MIDMEM, HIGHMEM)...

lieron by Associate
  • 2062 Views
  • 1 replies
  • 0 kudos

Resolved! Cypher using AES 128 CTR

Hi,Im trying to encryp using AES 128 CTR but i dont get the same result that online calculators.Im using this online calculator: https://cryptii.com/pipes/aes-encryptionMy code is the next:uint8_t IVKey[] = {0xDD, 0xF9, 0x11, 0xA6, 0xDD, 0xF9, 0x11, ...

Dosan by Associate III
  • 9102 Views
  • 11 replies
  • 2 kudos

STM32WB linker file

I'm having issues with a project based on an STM32WB5MM where some devices fail to operate BLE (like advertising, for example). The project integrates SBSFU and BLE_ota. I'm reviewing the linker files and I see differences in the management of the BL...

TFM / CubeMX integration and debugging

HI,we are interested in a guide to  a clear workflow of integrating CubeMX-generated code for U5 into TFM-based application.In particular:1. We have trustzone-enabled CubeMX-generated app with Azure RTOS and TouchGFX. The IDE and compiler are IAR. We...

bear2023R by Associate III
  • 1054 Views
  • 0 replies
  • 0 kudos

How to build SBSFU in team city build agent

Hi Team,I am working on project in which we are implementing Secure software upgrade feature using SBSFU. locally I am building SBSFU package, but our project follows different process. To meet that I need to build SBSFU package in TeamCity.could any...

jsalg.1 by Associate III
  • 955 Views
  • 1 replies
  • 0 kudos

STSAFE

Hi,How to authenticate a  device connected to STM 32 using USB Peripheral the STM 32 is integrated with STSAFE  IC , How to use peripheral Authentication Example for this in the software package 

SBSFU integration with STM32 L496ZG

I am integrating SBSFU with the STM32L496ZG microcontroller and have created a new project. I attempted to generate the SFB file using a customized post-build script from the L476 Simple App example. Although I modified the script paths for my projec...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.