2024-10-13 11:28 PM
Hi,
How to authenticate a device connected to STM 32 using USB Peripheral the STM 32 is integrated with STSAFE IC , How to use peripheral Authentication Example for this in the software package
2024-10-16 7:53 AM
Hi @jijomathew ,
I'm not sure to understand your request ?
You want to authenticate a USB device connected to your STM32 device USB port ?
In your STM32 device you have an STSAFE-A and is acting as USB master ?
Best Regards,
Benjamin
2024-10-16 10:44 PM
yes, Sir,
I want to try the peripheral authentication, in my STM 32, I have integrated STSAFE-A, and acting as a USB master.
Thanks and Regards
Jijo Mathew
2024-10-17 4:58 AM
Hi @jijomathew ,
The STSAFE-A shall on the side of the peripheral you want to authenticate in that case.
Having the STSAFE-A on the USB master side will enable mutual authentication with peripheral.
The code example provided in the X-CUBE-SAFEA1 is showcasing the authentication of the STSAFE-A by the STM32. The use case is that STSAFE-A is on the peripheral side an when plugged to the I2C of the STM32, the authentication is done.
Best Regards,
Benjamin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.