2025-02-27 11:57 PM - edited 2025-02-27 11:58 PM
I am implementing encryption and decryption using AES-GCM mode on the STM32 NUCLEO-U5A5ZJ-Q.
I have successfully encrypted and decrypted the string "Hello", but I am having issues with tag authentication.
I am using the function HAL_CRYPEx_AESGCM_GenerateAuthTAG to obtain the tag after the encyption process.
However, I cannot find a function to verify the tag.
I have two questions:
I obtained the tags from both the encryption and decryption processes, but different values were returned. Below is a portion of the implemented source code.
#define AES_KEY_SIZE 16
#define AES_IV_SIZE 12
#define AES_TAG_SIZE 16
CRYP_HandleTypeDef hcryp;
uint8_t aesKey[AES_KEY_SIZE] = {0x11, 0x11, 0x22, 0x22, 0x33, 0x33, 0x44, 0x44, 0x55, 0x55, 0x66, 0x66, 0x77, 0x77, 0x88, 0x88};
uint8_t aesIV[AES_IV_SIZE] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0a, 0x0b};
uint8_t plaintext[] = "Hello";
uint8_t ciphertext[sizeof(plaintext)];
uint8_t decryptedtext[sizeof(plaintext)];
uint8_t tag[AES_TAG_SIZE];
void AES_GCM_Encrypt(void)
{
HAL_StatusTypeDef status;
HAL_CRYP_DeInit(&hcryp);
hcryp.Instance = AES;
hcryp.Init.DataType = CRYP_DATATYPE_8B;
hcryp.Init.KeySize = CRYP_KEYSIZE_128B;
hcryp.Init.Algorithm = CRYP_AES_GCM_GMAC;
hcryp.Init.pKey = (uint32_t *)aesKey;
hcryp.Init.pInitVect = (uint32_t *)aesIV;
hcryp.Init.HeaderSize = 0;
hcryp.Init.Header = NULL;
hcryp.Init.DataWidthUnit = CRYP_DATAWIDTHUNIT_BYTE;
status = HAL_CRYP_Init(&hcryp);
if (status != HAL_OK)
{
printf("AES Init Failed\r\n");
return;
}
status = HAL_CRYP_Encrypt(&hcryp,
(uint32_t *)plaintext,
(uint16_t)sizeof(plaintext),
(uint32_t *)ciphertext,
HAL_MAX_DELAY);
if (status != HAL_OK)
{
printf("Encryption Failed\r\n");
return;
}
status = HAL_CRYPEx_AESGCM_GenerateAuthTAG(&hcryp, (uint32_t *)tag, HAL_MAX_DELAY);
if (status != HAL_OK)
{
printf("Auth Tag Generation Failed\r\n");
return;
}
printf("Encryption Success!\r\n");
}
void AES_GCM_Decrypt(void)
{
HAL_StatusTypeDef status;
uint8_t _tag[AES_TAG_SIZE];
HAL_CRYP_DeInit(&hcryp);
hcryp.Instance = AES;
hcryp.Init.DataType = CRYP_DATATYPE_8B;
hcryp.Init.KeySize = CRYP_KEYSIZE_128B;
hcryp.Init.Algorithm = CRYP_AES_GCM_GMAC;
hcryp.Init.pKey = (uint32_t *)aesKey;
hcryp.Init.pInitVect = (uint32_t *)aesIV;
hcryp.Init.HeaderSize = 0;
hcryp.Init.Header = NULL;
hcryp.Init.DataWidthUnit = CRYP_DATAWIDTHUNIT_BYTE;
status = HAL_CRYP_Init(&hcryp);
if (status != HAL_OK)
{
printf("AES Init Failed\r\n");
return;
}
status = HAL_CRYP_Decrypt(&hcryp,
(uint32_t *)ciphertext,
(uint16_t)sizeof(ciphertext),
(uint32_t *)decryptedtext,
HAL_MAX_DELAY);
if (status != HAL_OK)
{
printf("Decryption Failed\r\n");
return;
}
status = HAL_CRYPEx_AESGCM_GenerateAuthTAG(&hcryp, (uint32_t *)_tag, HAL_MAX_DELAY);
if (status != HAL_OK)
{
printf("Auth Tag Generation Failed\r\n");
return;
}
// The values of `tag` and `_tag` do not match here.
if (memcmp(tag, _tag, AES_TAG_SIZE) != 0) {
printf("Auth Tag mismatch\r\n");
return;
}
printf("Decryption Success! Decrypted Text: %s\r\n", decryptedtext);
}
int main(void)
{
// ...
AES_GCM_Encrypt();
AES_GCM_Decrypt();
// ...
}
Thank you in advance for your assitance.
Solved! Go to Solution.
2025-02-28 9:44 AM
Hello @y_yamamoto ,
yes TAG verification should be done using a memory comparison on your side.
Please check example:
STM32Cube_FW_U5_V1.7.0\Projects\B-U585I-IOT02A\Examples\CRYP\CRYP_AES_GCM\
Best regards
Jocelyn
2025-02-28 9:44 AM
Hello @y_yamamoto ,
yes TAG verification should be done using a memory comparison on your side.
Please check example:
STM32Cube_FW_U5_V1.7.0\Projects\B-U585I-IOT02A\Examples\CRYP\CRYP_AES_GCM\
Best regards
Jocelyn
2025-03-02 10:45 PM
Thank you for your response.
I understand that I need to implement the tag verification myself using memory comparion.
Additionally, after reviewing the sample code, I identified the cause of the tag mismatch during encryption and decryption. The size of the plaintext being encrypted was not a multiple of 16 bytes.
Thank you very much for your assistance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.