STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I2C firmware upload issue on RDP L1

Hello dear friends,this is my first post and I need your help with an issue I have. I designed some devices based on STM32C031C6. I use an I2C command to jump to bootloader and I upload the new firmware via I2C also from a microcomputer using the stm...

STM32H753 hardware crypto CCM failure

Hello, I've got STM32H53 MCU and trying to use hardware CCM accelerator as alternative CCM for mbedtls library.I've took HAL implementation from the repository STM32Cube_FW_H7_V1.11.2/Projects/STM32H743I-EVAL/Applications/mbedTLS/Crypto_Selftest/Src/...

AKali by Associate II
  • 1062 Views
  • 1 replies
  • 0 kudos

Resolved! Issue Integrating FreeRTOS with Secure Manager on STM32H5

Hello,I am new to the STM32 development environment and real-time programming. I have the STM32H573I-DK development board and have followed the workshop provided by ST, available on the wiki:https://wiki.stmicroelectronics.cn/stm32mcu/wiki/Security:H...

rtc.png Freertos_error.png erreor.png
Musa2 by Associate II
  • 4144 Views
  • 4 replies
  • 4 kudos

How to use STM_provisioning

I am using X-CUBE-MATTER v1.1.1. I understand that it is possible to use the DAC and PAI provided by CommScope using the project STM_provisioning. Please tell me more about STM_provisioning. Also, please tell me how to create STM_provisioning in ligh...

Resolved! Core Locked Up (STM32h753ZI)

Hi,I am Working on SBSFU. I have Flashed the STM32H753zi example code after flashing i am not able to flash from programmer. even after changing the option bytes RDP level 0 is set.I have Connect another working board of stm32h753zi board i compared ...

Prakash_Raj1994_1-1737700720445.png Prakash_Raj1994_0-1737700331833.png

Readout protection of OBK-Keys from user software

Hello.If i set the product state to CLOSED (0x72)  without TZ-enabled (TZEN: 0xC3),i can't access the device and the OBK-Keystore from outside.But if i write a user program, i can read the whole OBK-Keystore at:FLASH_OBK_BASE_S + 0x0100;So perhaps it...

Resolved! OEMiROT for STM32H523 MCU

Hi, I am working on OEMiROT bootloader for STM32H523. I have copied big parts of the ST OEMiROT example project from H533 example as this is the closest MCU to H523 from the flash memory layout perspectives. However, it is taking ridiculously too lon...

hakeila by Associate III
  • 6112 Views
  • 10 replies
  • 1 kudos

mbedTLS on STM32U575CGUx

Hi, There is a lot of differing documentation w.r.t the use of mbedTLS for STM32U5 MUC. Can someone share an "Application Note" or any documentation which explains the integration of mbedTLS library in the project. PS: The relevant configuration file...

Chinmay by Associate
  • 1866 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.