STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [STM32L081xx] __HAL_RCC_AES_CLK_ENABLE missing

Hi all,I generated code in STM32CubeMX for STM32L081CBTx controller with AES enabled.I built the generated code (without modification) in STM32CubeIDE, but it failed with warning:../Core/Src/stm32l0xx_hal_msp.c: In function 'HAL_CRYP_MspInit': ../Cor...

ISzik.1 by Associate
  • 2352 Views
  • 2 replies
  • 0 kudos

Code does not run when RDP is enabled on STM32L072

Hi ST community,I have a fully functional application on my STM32L072. The problem is when I tried to enable RDP, nothing works anymore.After flashing the application I tried to connect with ST-Link, the option bytes are set correctly and it is not p...

RCont.1 by Associate II
  • 936 Views
  • 0 replies
  • 1 kudos

Read protection on STM32 chip

Read Protection has been set in the STM32 chip .In this case, how to judge the chip is in the read protection state through the bootloader program of the chip.I now is to send the erase instruction, if return NACK, judge chip is in the read Protectio...

忠余.1 by Associate II
  • 2181 Views
  • 5 replies
  • 0 kudos

About CRCSIZE setting in STM32H7 SPI peripheral

I am confused about the setting of the SPI CRC functionality: it is not clear what CRCSIZE is doing and how to set it. I understand that to get a N bits CRC you have to choose a N+1 bits polynom, but why is the length of the CRC not deduced from the ...

Gpeti by Senior II
  • 1159 Views
  • 3 replies
  • 0 kudos

what will be the source file path for x-cube-cryptolib-master for AES256 Encryption . I Used Atollic truestudio for CubeMax gererated code. I Download x-cube-cryptolib-master from ST.com

Not able to access some function definition for AES256 . I am using Atolic true studio for cubeMx generated Code. I used STM32L442KC MicrocontrollerI Added crypto library using below steps .open properties of project and in C/C++ general>Paths and Sy...

STAR by Associate II
  • 807 Views
  • 0 replies
  • 0 kudos

Resolved! Should SFU_LL_Flash_Write be aligned to 64 or 32 bit?

In the code it says the following:/** * @brief This function writes a data buffer in flash (data are 32-bit aligned). * @note After writing data buffer, the flash content is checked. * @param pFlashStatus: FLASH_StatusTypeDef * @param pD...

Arno1 by Senior
  • 1284 Views
  • 1 replies
  • 0 kudos

Resolved! Require authentication for firmware update

I started a new project, and my security requirement states that user authentication is required when updating firmware.I wonder if there's a feature for this, and if not, can the bootload side be modified to meet this requirement?I searched and foun...

DPark.2 by Associate II
  • 2621 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.