STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 signing tool problem with image size

There is a problem with STM32 signing tool version 2.21.0. When header version is 2.3 and alignment flag is used, then image length in header is greater by the alignment byte count.To reproduce:Create dummy.bin that is filled with 256 bytes of FF's. ...

dummy.png signed.png

STM32N6 FSBL digital signature public keys

I read UM3451 (STM32N6xx security guidance for SESIP level 3 certification) chapter 3.2.2 Secure installation and I wonder why aren't the FSBL signature public keys not written into OTP fuses? Only the 8 words (32 bytes) of hashes of all 8 public key...

Resolved! STiROT + OEMuROT for STM32H7S: feedback

We've been using STiROT + OEMuROT for STM32H7S on our system, with our own application.The secure bootloader handles most of its functionality very well, and the security aspects in particular. The scripts provided by ST were very helpful, as was the...

Resolved! Unable to regress to RDP=0

I'm working on a custom STM32U5 board and I'm trying to harden the system.I followed the AN5347 (https://www.st.com/resource/en/application_note/an5347-arm-trustzone-features-for-stm32l5-and-stm32u5-series-stmicroelectronics.pdf) in particular I foll...

Resolved! How to properly regenerate Keys for SM project

When creating a new project (for STM32H573) using CubeMX, it generates defaults keys under ROT_Provisioning\SM\Keys:06/19/2025 03:20 PM 232 ITS_key1.pem02/17/2026 09:34 PM 16 SFI_Encryption_Key.bin02/17/2026 09:34 PM 12 SFI_Encryption_Nonce.bin02/18/...

Thatseasy by Associate III
  • 998 Views
  • 9 replies
  • 1 kudos

secure boot and secure firmware update for STM32H750 MCU

We need the secure boot and secure firmware update solution for both the execution models to meet the EU-CRA standard:• Execute in place support (XiP support) - direct execute from external QSPI flash• BootROM support - copy from QSPI flash to SDRAM,...

ckw089 by Associate II
  • 298 Views
  • 2 replies
  • 0 kudos

port mcuboot demo app to custom board

Have successfully worked throughSTM32Cube_FW_U5_V1.8.0/Projects/B-U585I-IOT02A/Applications/SBSFU/readme.htmlI need to port this (..boot, ..loader, ..appli) to a custom board running STM32U585VIT6.Within the readme it states "This example has been te...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.