2026-02-22 11:31 PM
Hello ST Support,
I reproduced an ETH TX DMA issue on STM32N6570-DK where the DMA never consumes the TX descriptor.
Environment
- Board: STM32N6570-DK
- Security: TrustZone enabled, Secure-only platform configuration
- PHY: ID1=0x001C, ID2=0xC916, link-up confirmed
- Interface: RGMII, 1G link
Observed behavior
- HAL_ETH_Transmit*() submit succeeds (st=0)
- TX descriptor OWN bit remains 1 (never cleared by DMA)
- TX complete callback/counter never increments
- DMA enters/keeps TBU state
- Key symptom: DMACCATXBR remains 0 (buffer base is never loaded)
Representative logs
- [eth][post-start] dlar=0x3402C1E0 dtpr=0x3402C1E0 rlr=0x00000003 txcr=0x00200001 dmacc=0x00080218 txqomr=0x0007000A
- [tx][path] st=0 own=0->1 catxdr=0x3402C1E0->0x3402C1E0 catxbr=0x00000000->0x00000000 csr=0x00000000->0x00000004
- [tx][stall] own=1 ... catxdr=0x3402C1E0 catxbr=0x00000000 csr=0x00000004 ... dmad=0x00006400 tps0=0x00006000 axr=0
axw=0
What we already tried (same result in all cases)
1. EDSE on/off (txcr=0x10200001 / 0x00200001)
2. DSL forced/unforced (0/64-bit skip)
3. Descriptor/buffer placement changes:
- ETHRAM (0x341F8xxx)
- AXI SRAM (0x3402xxxx, non-cacheable)
4. RIFSC/RISAF adjustments:
- forced RIMC_ATTR secure/privileged attributes
- widened RISAF2/RISAF6 region permissions
5. CH0-only bring-up attempts, CH1 disabled/separated
6. TBU clear + re-kick (rewrite DTPR)
7. Manual single-descriptor ring probe (DTPR=DLAR and DTPR=DLAR+stride)
Additional notes
- RIMC_ATTR sweep over indices 0..12 produced no hit
- RISAF illegal access latches show no meaningful fault for this path
- No meaningful AXI read/write error status (AXRHSTS/AXWHSTS=0)
Questions
1. On STM32N657, is ETH DMA outbound security attribute control actually under RIFSC RIMC_ATTR?
2. What is the exact outbound master index/mapping for ETH DMA?
3. Is there any known limitation/errata for ETH DMA descriptor fetch in Secure-only configurations?
4. Do you have a recommended initialization sequence for the pattern:
CATXBR=0 + TBU + OWN stuck?
Solved! Go to Solution.
2026-02-26 2:15 AM
Hi @Ricky_Jeon
You can find it here.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-23 2:54 AM
Hi @Ricky_Jeon
Would you attach minimum firmware to reproduce the issue?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-24 12:10 AM
Hello ST Support Team,
I’m seeing a persistent ETH DMA TX stall on STM32N6570-DK and would like your help analyzing the root cause.
Repro project (minimal, ETH/FreeRTOS focused):
https://github.com/RickyJeon97/STM32N6570DK_ETH_DMA.git
Issue summary:
- PHY link comes up correctly.
- TX descriptor OWN bit remains set (own=1) and TX does not progress.
- DMA status is stable at csr=0x00000004.
- AXI fault counters remain zero (axr=0, axw=0).
Representative log:
[phy] addr=0 id1=0x001C id2=0xC916
[eth][dsl] forced DSL=0
[eth][txq0] qomr 0x0007000A->0x00070006
[eth][post-start] dlar=0x3402B0C0 dtpr=0x3402B0C0 rlr=0x00000003 txcr=0x00200001 dmacc=0x00000218 txqomr=0x00070006
[phy] link up (addr=0 bmsr=0x79AD)
[tx][stall] own=1 csr=0x00000004 catxdr=0x3402B0C0 catxbr=0x00000000 dlar=0x3402B0C0 dtpr=0x3402B0C0 d0=0x3402C000
d3=0xB000003C dmad=0x00006400 axr=0 axw=0
[focus] txdesc_s=0x3402B0C0 txdesc_ns=0x2402B0C0 txbuf_s=0x3402C000 txbuf_ns=0x2402C000
[tx][tdtA] rlr=0x00000003 stride=0x18 dtpr=0x3402B0C0 catxbr=0x00000000 dmad=0x00006400
[tx][tdtB] rlr=0x00000003 stride=0x18 dtpr=0x3402B108 catxbr=0x00000000 dmad=0x00006400
What I need help with:
1. Is this register/descriptor state indicating a known configuration issue?
2. Are there specific ETH DMA/MTL/MAC settings on STM32N657 that can cause TX OWN to never clear in this state?
3. Any recommended debug checkpoints (registers or sequence) for CH0 TX descriptor fetch/advance?
Thanks in advance for your guidance.
2026-02-25 4:56 AM
Hi @Ricky_Jeon
Your project doesn't seem to be similar to the reference projects.
The fastest way to narrow down the root cause is to:
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-25 3:19 PM - edited 2026-02-25 4:11 PM
2026-02-26 2:15 AM
Hi @Ricky_Jeon
You can find it here.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-26 3:21 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.