STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SBSFU [SBOOT] System Security Check failed

Device: STM32L4S5Trying to run x-cube-aws v2.2.1I've successfully flashed the B-L4S5I-IOT01_STSAFE_Provisioning binary (output below)Start provisioning of STSAFE-A   Force STSAFE-A provisioning   Launching STSAFE-A pairing Check if Pairing Host keys...

DAzev.1 by Associate
  • 1653 Views
  • 1 replies
  • 0 kudos

Resolved! B-U585I-IOT02A definitely locked?

Hello STM32U5 community,I was making a few attemps with my B-U585I-IOT02A demo board and TF-M. I am afraid I have irreversibly locked the MCU.Here is what I did:run regression.shset RDP level 1 with the Programmer despite the warnings, because I forg...

ELuca.2 by Associate II
  • 2552 Views
  • 3 replies
  • 0 kudos

Issue with AES and CKS

In my application, I have a sequence which looks something like this:Load an AES key from CKS using SHCI_C2_FUS_LoadUsrKeyCall HAL_Cryp_Init, HAL_Cryp_Decrypt, and HAL_Cryp_DeInit to decrypt a block of dataUnload the key from CKS using SHCI_C2_FUS_Un...

crwper by Senior
  • 2732 Views
  • 6 replies
  • 0 kudos

RSA support for X509 utilities

Hi,I'm using some STM32 drivers code to parse X509 certificates. These drivers are based on ECC cryptography. I need to change to RSA. I need utilities such as parseCert()isValidCert()isParent()which exist for ECC, but I cannot find any equivalents f...

FOCal.1 by Associate
  • 1728 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.