2022-11-21 2:53 AM
Hi ST Team,
I'm working on a project where I'm using SBSFU as bootloader (on a STM32H7). When I download the new firmware image, SBSFU reboot the system and start execution (decrypting image, validating and so on...). While SBSFU is doing these actions I would like to update a simple display that is made by 7-segment LEDs, so I need to manage it inside an interrupt routine. I notice that when the code jumps inside SECore code it disables the interrupt for a long time causes flickering on the display.
How can I manage that situation?
Thanks a lot in advance?
GDV
2022-11-28 3:09 AM
Hi @Giulio Dalla Vecchia,
the SBSFU is programing flash. It's quite normal that access to flash (same bank) is stalled several milliseconds during the write operation.
I think that with the latest SBSFU it should already be possible to place ISR (and vector table) into SRAM. This should solve your problem.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.