2022-11-30 8:54 AM
Device: STM32L4S5
Trying to run x-cube-aws v2.2.1
I've successfully flashed the B-L4S5I-IOT01_STSAFE_Provisioning binary (output below)
Start provisioning of STSAFE-A
Force STSAFE-A provisioning
Launching STSAFE-A pairing
Check if Pairing Host keys available
Pairing OK
Erase Data : OK
Now Store Certificate STM_POC_SBSFU_ROOT_TEST_CA_00 inside STSAFE-A
Certificate STM_POC_SBSFU_ROOT_TEST_CA_00 successfully written inside STSAFE-A : OK
Now Store Certificate STM_POC_SBSFU_OEM_TEST_CA_00 inside STSAFE-A
Certificate STM_POC_SBSFU_OEM_TEST_CA_00 successfully written inside STSAFE-A : OK
Now reading and compare Certificates written inside STSAFE-A :
Get Certificate CERT_CA_FW OK
Certificate CERT_CA_FW successfuly read and compared : OK
Get Certificate CERT_CA_OEM_FW OK
Certificate CERT_CA_OEM_FW successfuly read and compared : OK
End provisioning of STSAFE-A The next step, which was to flash SBSFU results in the following
= [SBOOT] System Security Check failed! Rebooting…
========= End of Execution ==========
= [SBOOT] System Security Check failed! Rebooting…
========= End of Execution ==========
= [SBOOT] System Security Check failed! Rebooting…
========= End of Execution ==========How can I troubleshoot this?
2022-11-30 9:57 AM
Ok, I was able to progress by unchecking the DBANK user option configuration.
now I get this
= [SBOOT] System Security Check successfully passed. Starting…
======================================================================
= (C) COPYRIGHT 2017 STMicroelectronics =
= =
= Secure Boot and Secure Firmware Update =
======================================================================
= [SBOOT] STATE: WARNING: SECURE ENGINE INITIALIZATION WITH FACTORY DEFAULT VALUES!
= [SBOOT] STATE: CHECK STATUS ON RESET
INFO: A Reboot has been triggered by a Software reset!
INFO: Last execution detected error was: No error. Success.
= [SBOOT] STATE: CHECK NEW FIRMWARE TO DOWNLOAD
= [SBOOT] STATE: CHECK KMS BLOB TO INSTALL
= [SBOOT] STATE: CHECK USER FW STATUS
Slot SLOT_ACTIVE_1 not empty : erasing …
No valid FW found in the active slots nor new FW to be installed
Waiting for the local download to start…
= [SBOOT] STATE: DOWNLOAD NEW USER FIRMWARE
File> Transfer> YMODEM> Send C.C.CBut when I download the aws_demo.bin file, I stop getting serial output... Again, stuck with no troubleshooting output.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.