2022-10-05 4:47 AM
Hi,
I'm using some STM32 drivers code to parse X509 certificates. These drivers are based on ECC cryptography. I need to change to RSA. I need utilities such as
parseCert()
isValidCert()
isParent()
which exist for ECC, but I cannot find any equivalents for RSA cryptography.
Specifically, I need to check a chain of trust of RSA certificates, and I also need to call RSA_PKCS1v15_Verify() for an RSA signature, so I need to pass in the public key in a structure RSApubKey_stt, and this has to be extracted from the leaf certificate.
The target MCU is STM32H753.
The ECC-based X509 utilties I'm working with are dated 24-february-2017.
Do such utilities exist for RSA? Or do I have to write them myself?
Thanks
2022-11-16 6:02 AM
Hi @FOCal.1,
there are various crypto libraries including the X509, I think the most popular is mbed crypto, used for example also in our X-CUBE-SBSFU (SBSFU makes no use of x509, but the library it uses has this capability).
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.