STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! how to set PCROP Protection to default STM32H755

hello ST Community,I'm trying to protect sector 0 of the flash drive from mass erasure using the PCCOP Protection option on the NUCLEO-H755ZI-Q.After tinkering around a bit to understand its functions, I can no longer reset its protection to its defa...

image.png image.png
Domy_ST by Senior
  • 940 Views
  • 14 replies
  • 6 kudos

SBSFU 2.8 - Installation does not resume

Hello,I'm currently integrating the SBSFU 2.8 for one of our board, that use a STM32H753, with a dual-slot configuration.I'm adapting the example for the STM32H753ZI. For now, this mostly involves modifying the USART (use the 6 instead of the 3).I am...

Interrupts in SBSFU for STM32F429

Hello, I've recently managed to modify the SBSFU example for the STM32F413H-Discovery board and adapt it for my STM32F419 mcu, building it and executing it successfully.Now the issue is, i need to modify the loading mode from serial ymodem to downloa...

fstaffa by Associate
  • 151 Views
  • 0 replies
  • 0 kudos

GPIO_IOToggle_TrustZone example using STM32 TrustZone

Hi everyone,I’m currently experimenting with the GPIO_IOToggle_TrustZone example using STM32 TrustZone.When I build and flash both the Secure and NonSecure firmware, everything works correctly: the LED toggles as expected, so the interaction between ...

stst9187 by Associate III
  • 285 Views
  • 2 replies
  • 1 kudos

STM32H5 - Secure Manager - BusFault

Hello,long time lurker, now with an issue that I would like to solve. I developed a firmware that runs standalone without issue. I would like to use the secure manager on my STM32H573VI microcontroller.I followed the procedures at this link: https://...

OEMiRoT – S-only application (no TrustZone isolation): correct configuration of MCUBOOT_APP_IMAGE_NUMBER and FLASH_NS_PARTITION_SIZE

 Hi,I am working with the OEMiRoT reference project (STM32U385) and I need to configure a single Secure application image without TrustZone isolation (S-only application), while still keeping the Secure Data Image enabled.From flash_layout.h, I see t...

stst9187 by Associate III
  • 120 Views
  • 0 replies
  • 0 kudos

STM32H563: Unable to detect DBGMCU Mailbox ST

Hi,On a custom board I get the following message: Unable to detect DBGMCU Mailbox STwhen i run regression.bat.I did several test (provisionning, regression) before and i didn't notice any issuesDA with password and TZ disabledA program is running on ...

gh_rcl_0-1777541862602.png
gh_rcl by Associate II
  • 298 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.