2024-11-14 6:38 PM
Hi there,
There is a config option named "OB_STOP_RST" that exists in Option Bytes' USERconfig, I tested it with STOP mode, and it works well.
But I can't understand when we should use it. After clearing this bit to OB_STOP_RST, the MCU will reset right away and enter run mode when it enters stop mode, why don't we just reset the MCU, it's easier and faster.
Same as the OB_STDBY_RST config.
Solved! Go to Solution.
2024-11-15 2:43 AM
Hello @Junde,
This can be useful in scenarios where the system needs to ensure a clean start after waking up from STOP mode, avoiding any potential issues that might arise from an improper wake-up sequence or corrupted state
>>why don't we just reset the MCU, it's easier and faster
these OB provide a controlled way to handle low-power mode entries, instead of relying on external events or manual resets.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-15 2:43 AM
Hello @Junde,
This can be useful in scenarios where the system needs to ensure a clean start after waking up from STOP mode, avoiding any potential issues that might arise from an improper wake-up sequence or corrupted state
>>why don't we just reset the MCU, it's easier and faster
these OB provide a controlled way to handle low-power mode entries, instead of relying on external events or manual resets.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-18 10:18 PM
I got it, thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.