STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 UART Byte-to-Byte treatment

Hello, I am trying to receive and transmit byte-to-byte on a STM32F429 Discovery, I will be using a STM32U5 Discovery soon. I used UART IT method but maybe there is a better solution...Objective & Issue:I want to continuously receive and send byte-to...

Nero by Associate II
  • 3099 Views
  • 4 replies
  • 7 kudos

How to clear the specified flash page's WRP?

Hi there,I want to clear the specified flash page's WRP by program, but I can only do it by clearing all the flash page's WRP,meanwhile, I also need to keep my data in option byte.my code is as follows(the project at HERE :(uint8_t data0 = HAL_FLASHE...

Junde by Senior III
  • 1835 Views
  • 2 replies
  • 0 kudos

Resolved! when we should use the OB_STOP_RST config in Option Bytes?

Hi there,There is a config option named "OB_STOP_RST" that exists in Option Bytes' USERconfig, I tested it with STOP mode, and it works well.But I can't understand when we should use it. After clearing this bit to OB_STOP_RST, the MCU will reset righ...

Junde by Senior III
  • 1547 Views
  • 2 replies
  • 1 kudos

SSD1963 with STM32F407 using FSMC

Hello,I am trying to configure STM32F407VGT6 discovery to work with 800x480 LCD with SSD1963 onboard. In the end i would like to use TouchGFX to run the GUI.I was testing several configurations to display anything manually first. It looks like the co...

oleq96 by Associate
  • 1934 Views
  • 1 replies
  • 0 kudos

SMPS fail to supply Vcore, what could be happen?

Hi, I'm using a STM32H757XIH6 with SMPS. Everything (firmware & hardware) are working fine but after a switch off/on of the power supply, I could not connect to the microcontroler via SWD. First I thought it was the Power configuration that had been ...

Byann.1 by Associate II
  • 5460 Views
  • 4 replies
  • 0 kudos

STM32L431RCT6 wakes up immediately after standby

I am trying to use STM32L431RCT6 with STM32CubeIDE and STM32Cube_FW_L4_V1.18.1 for a low power mode application. I tried Sleep mode, Stop mode and they both work OK. But the standby mode does not working. The MCU wakes up instantly after entering sta...

NEdom1_1-1731950055328.png
NEdom.1 by Associate III
  • 1958 Views
  • 3 replies
  • 0 kudos

STSW-LINK009 Driver Install Fail

Hello, I am on a MacBook Pro M2 running Parallels Windows 11. I have downloaded the STSW-LINK009 zip file. Because of my machine, I need to run the dpinst_amd64.exe file. It opens and runs perfectly fine but I am unable to install the drivers as it s...

Driver Install Fail.png
alan29 by Associate
  • 11617 Views
  • 3 replies
  • 0 kudos

STM32_Programmer_CLI fails to flash

Using the STM32 CLI on Windows:STM32_Programmer_CLI.exe c port=swd reset=HWrst -e all -d my_filename.hex -v -s -g This just prints: If I remove the -d option, it performs the erase, so I know it can talk to the chip.  I have tried the verbosity optio...

JBill10_0-1731965731898.png
JBill.10 by Associate III
  • 855 Views
  • 1 replies
  • 0 kudos

Resolved! RCC stuck!

hey thereI have a customized board with STM32F030K6T6 on it and a 11.0592MHz crystal for HSE. the thing is my code does not run through and when I try to debug it, I can see it sticks in SystemClock_Config(), more specifically, in HAL_RCC_OscConfig()...

Ala by Senior
  • 5356 Views
  • 8 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.