2017-11-25 1:05 PM
Hi, I am working in stm32f746 discovery board. I want to drive the Lcd. At initialize step, I have to use the BSP_LCD_LayerDefaultInit(uint16_t layerIndex, uint32_t FB_Address).
I dont know what is FB_Address?
Can any body introduce a document to help me?
Tanks.
2017-11-25 1:30 PM
FB - Frame Buffer
Address within STM32 address space you are using to describe screen content. ie 0xC0000000 would be base of SDRAM in some implementations.
2017-11-25 1:40 PM
The driver is well-commented. Read the source fileSTM32Cube_FW_F7_V1.8.0/Drivers/BSP/STM32746G-Discovery/stm32746g_discovery_lcd.c
FB_Address is the address of where you put your frame buffer in memory. I don't have your exact board, but on the f769-discovery, I use the external sdram for the frame buffer.
Looks like the 746 is the same way. look in STM32Cube_FW_F7_V1.8.0/Drivers/BSP/STM32746G-Discovery/stm32746g_discovery_lcd.h and note this:
#define LCD_FB_START_ADDRESS ((uint32_t)0xC0000000)
here's how I do it on stm32f769i-discovery:
static void LCD_Config(void)
{
uint8_t lcd_status = LCD_OK;
uint8_t lcd_brightness[] = {OTM8009A_CMD_WRDISBV, 0xFF};
/* LCD DSI initialization in mode Video Burst */
/* Initialize DSI LCD */
BSP_LCD_Init();
while(lcd_status != LCD_OK);
DSI_IO_WriteCmd(0, (uint8_t *)lcd_brightness);
BSP_LCD_LayerDefaultInit(LTDC_ACTIVE_LAYER_BACKGROUND, LCD_FB_START_ADDRESS);
/* Select the LCD Background Layer */
BSP_LCD_SelectLayer(LTDC_ACTIVE_LAYER_BACKGROUND);
/* Clear the Background Layer */
BSP_LCD_Clear(LCD_COLOR_BLACK);
BSP_LCD_LayerDefaultInit(LTDC_ACTIVE_LAYER_FOREGROUND, LCD_BG_LAYER_ADDRESS);
/* Select the LCD Foreground Layer */
BSP_LCD_SelectLayer(LTDC_ACTIVE_LAYER_FOREGROUND);
/* Clear the Foreground Layer */
BSP_LCD_Clear(LCD_COLOR_BLACK);
/* Configure the transparency for foreground and background :
Increase the transparency */
BSP_LCD_SetTransparency(LTDC_ACTIVE_LAYER_BACKGROUND, 0);
BSP_LCD_SetTransparency(LTDC_ACTIVE_LAYER_FOREGROUND, 255);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
The DSI_IO_WriteCmd is just to kill the whine it makes when not at full brightness
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.