2015-09-21 2:59 AM
Hello,
i have a very dangerous bug in CubeMx with HRTIM module (STM32F334C8). Sometimes the dead times are not inserted on the outputs. The configuration is done correctly but in the source file hrtim.c only the dead times for the timer A or B are set in the corresponding registers. The timer C is sometimes not set for the dead times. When it arrives the only solution is to create a new project.I have to drive motors or SMPS and this bug affects the reliability of our future products.When i make a modification in my CubeMx project i must verify in the hrtim.c file that dead times are correctly set.I join a example project when the bug happens. In this case only the timer B outputs have a dead time inserted.Thanks in advance2015-09-30 2:45 AM
Hi Philippe,
Thank you for your feedback. The issue is under investigation by our development team. -Shahrzad-2016-01-28 2:43 AM
Hi Philippe,
The fix is already delivered in STM32CubeMX 4.12.0.-Shahrzad-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.