cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F042 USB VCP Example

caio
Associate
Posted on September 18, 2014 at 17:21

Hello everyone,

I'm trying to use the USB STM32F042, used as a base example STM32F072 USB-discovery, but the windows me answer the following error: This device can not start (code 10).

I wonder if anyone has any examples of VCP for this chip working, or why he does not connect ...

Any idea?

Thanks ...
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
rohanne
Associate II
Posted on January 13, 2015 at 12:11

I have the same problem. Have you anybody resolved this issue?

erisson
Associate II
Posted on January 15, 2015 at 14:00

Try editing the file (.inf)

replacing the names

usbser -> Serenum

And then add a new legacy driver

with this file.

rohanne
Associate II
Posted on January 15, 2015 at 17:54

I don't understand what you mean by adding a new legacy driver with the *.inf file. I renamed all of 

usbser

to

serenum

, then

I uninstalled the driver in Device Manager and re-pluged the usb connection -> then automatic driver instalation launched,

but finally message

''Device driver software was not succesfully installed'' showed up. So I still think it's the code matter.

The same issue solved here. Please, write there: 

https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fSTM32F04

2K6%20USB%20init%2e%20for%20VCP%20com&FolderCTID=0x01200200770978C69A1141439

FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2F

my%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2F

AllItems%2Easpx&currentviews=17

erisson
Associate II
rohanne
Associate II
Posted on January 21, 2015 at 13:39

I have already tried it - no effect. See the thread I posted above - I mention there everything I have tried.

yanvasilij
Associate II
Posted on January 28, 2016 at 11:44

Hello! Have you succed in creating usb project? Could you shere it? Regards

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.