STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Clock configuration

Posted on January 28, 2016 at 09:35Hi, i am designing a board based on f329. The problem is,   i have a red mark on the clock configuration on HSI(16MHZ) and also 48MHZ clocks. when i am configuration with HSI(16MHZ). Could anyone tell me why ?i hav...

arunease by Associate II
  • 1070 Views
  • 3 replies
  • 0 kudos

ST-Link + Level 1 read protection = bricked?

Posted on January 28, 2016 at 14:18Using IAR EWARM with ST-Link.I just set the protection level to Level 1 and now I cannot get in again to change the RDPRT  bits back to Level 0Any suggestions? #stm32f303x-read-protection

gbigden by Associate III
  • 1122 Views
  • 4 replies
  • 0 kudos

Cannot write to Memory on STM32F071V8

Posted on January 28, 2016 at 12:28Hi, I get the following error when trying to write to memory with the latest STLink Utility: 12:09:09 : ST-LINK SN : 48FF6E064967535727520587 12:09:09 : ST-LINK Firmware version : V2J25S4 12:09:09 : Connected via ...

STM32F042 USB VCP Example

Posted on September 18, 2014 at 17:21Hello everyone,I'm trying to use the USB STM32F042, used as a base example STM32F072 USB-discovery, but the windows me answer the following error: This device can not start (code 10).I wonder if anyone has any ex...

caio by Associate
  • 2473 Views
  • 6 replies
  • 0 kudos

Very dangerous bug with dead time insertion

Posted on September 21, 2015 at 11:59Hello,i have a very dangerous bug in CubeMx with HRTIM module (STM32F334C8). Sometimes the dead times are not inserted on the outputs. The configuration is done correctly but in the source file hrtim.c only the d...

HAL based ADC-DMA makes only one transaction

Posted on January 26, 2016 at 20:03 Hello. I try to make a simple non-continuous ADC-DMA transaction of 10 measurements. I get only one sample in my array. I don't use interrupts, just wait for DMA completion. Could you tell, what I am doing wrong...

baranovus by Associate III
  • 853 Views
  • 1 replies
  • 0 kudos

Bug report: USB CDC Template and CubeMX code generation

Posted on December 22, 2015 at 10:18Hi, I just created a new project for a STM32F103 MCU using CubeMX 4.12.0 and the firmware package 1.2.0 for the F1 family and came across two little issues. In Middlewares/ST/STM32_USB_Device_Library/Class/CDC/Src...

work by Associate II
  • 1679 Views
  • 3 replies
  • 0 kudos

STM32, mipi, CSI (mobile camera)

Posted on January 27, 2016 at 09:00Hello friends.Does anyone have any suggestions on the following topic?I found out that mobile cameras are very chip. For example iphone 4s 8M camera is about $2. But they use mipi interface (CSI-2, CSI-3). I would ...

baev_al by Associate III
  • 4195 Views
  • 1 replies
  • 0 kudos

Problems reconnecting virtual com port after software reset

Posted on January 26, 2016 at 10:03Hello all, I cannot reconnect COM port of a BLUENRG dongle after reseting. I call NVIC_SystemReset(), dongle resets, but cannot reopen same COM port to comunicate with device. I'm using latest Virtual COM Port driv...

vpalacio by Associate II
  • 997 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.