2021-11-03 4:07 AM
I have 3 ADCs (ADC1, ADC2, ADC3) configured with 3 different channels for 3 gpio pins to collect the data and all 3 ADC's are triggered simultaneously by TIM1 at the rising edge of the pulse.
It is also configured in the single conversion mode (i.e., at the rising edge of the pulse ADC's are triggered and conversions are made and it is stopped), it is working all good till here. but, when the continuous mode is enabled the ADC values are still triggered but the values getting is completley different (to be precise these values doesnot make any sense and kind of some random junk value).
so my question is, is it possible to configure ADC is continuous conversion mode and also trigger all the 3 ADC's simultaneously at the rising edge of pulse and collect the values after disabling the ADC's at some point?
// ADC's channel and gpio pin initializations.
cADCReadout::sADCInitStruct adc1;
adc1.ADCChannel = ADC1;
adc1.DMAChannel = DMA_Channel_0;
adc1.DMAStream = DMA2_Stream0;
adc1.DMATRSFCompleteFlag = DMA_FLAG_TEIF0;
cADCReadout::sADCInitStruct adc2;
adc2.ADCChannel = ADC2;
adc2.DMAChannel = DMA_Channel_1;
adc2.DMAStream = DMA2_Stream3;
adc2.DMATRSFCompleteFlag = DMA_FLAG_TEIF0;
cADCReadout::sADCInitStruct adc3;
adc3.ADCChannel = ADC3;
adc3.DMAChannel = DMA_Channel_2;
adc3.DMAStream = DMA2_Stream1;
adc3.DMATRSFCompleteFlag = DMA_FLAG_TEIF0;
m_oADC1.initialize(adc1);
m_oADC1.addChannel(GPIOA, GPIO_Pin_1,ADC_Channel_1,ADC_SampleTime_112Cycles);
m_oADC1.initialize(adc2);
m_oADC1.addChannel(GPIOA, GPIO_Pin_2,ADC_Channel_2,ADC_SampleTime_112Cycles);
m_oADC1.initialize(adc3);
m_oADC1.addChannel(GPIOA, GPIO_Pin_3,ADC_Channel_3,ADC_SampleTime_112Cycles);
//ADC and DMA configuartions
void cADCReadout::initialize(sADCInitStruct init)
{
m_sInitStruct = init;
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
DMA_InitTypeDef DMA_InitStructure;
//DMA
DMA_InitStructure.DMA_Channel = init.DMAChannel;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&(init.ADCChannel->DR);
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)(&m_aRecBuffer);
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = BUFFERSIZE; //It was 0 before
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(init.DMAStream, &DMA_InitStructure);
DMA_Cmd(init.DMAStream, ENABLE);
//ADC
ADC_CommonInitStructure.ADC_Mode = ADC_TripleMode_RegSimult;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInitStructure.ADC_DMAAccessMode =ADC_DMAAccessMode_1;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInit(&ADC_CommonInitStructure);
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_Rising ;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion =1;
ADC_Init(init.ADCChannel, &ADC_InitStructure);
ADC_EOCOnEachRegularChannelCmd(init.ADCChannel, DISABLE);
/* Enable DMA request after last transfer (Single-ADC mode) */
ADC_DMARequestAfterLastTransferCmd(init.ADCChannel, ENABLE);
}
2022-06-24 12:04 PM
Has anyone figured out a solution to this? I am also trying to start multiple ADCs with one timer trigger
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.