2026-02-24 2:43 AM - last edited on 2026-02-24 2:47 AM by Andrew Neil
Hello ST community,
I am working on an application on STM32N6570-DK using the camera to detect humans with an AI model (X-CUBE-AI + NPU) and draw bounding boxes on the LCD using LTDC.
I am facing a display corruption / glitch issue that only appears under very specific conditions, and I strongly suspect an AXI / interconnect / NPU side effect, possibly related to an undocumented reset or QoS state.
Project architecture:
Camera -> DCMIPP -> PIPE1 -> BUFFER1 -> LTDC_L1
-> PIPE2 -> BUFFER2 -> NPU -> Config ROI of DCMIPP
Memory placement:
LTDC framebuffer: AXIRAM2
AI input/output buffers: AXIRAM5
No buffer sharing between LTDC and AI
Problem description:
When MX_X_CUBE_AI_Process() is commented, the camera preview is perfectly stable on the LCD.
When MX_X_CUBE_AI_Process() is enabled, continuous display glitches appear (tearing / corrupted lines).
The issue happens only when LTDC is fetching the framebuffer while the NPU is running.
The camera can be fully desynchronized (snapshot mode, manual triggering), the issue still happens.
If I start one debug session (SWD):
The application runs perfectly
No display glitches at all
Even after:
leaving debug mode
software reset
The system keeps working until power is removed
After a power cycle, the issue reappears.
Questions:
Does the NPU act as a high-priority AXI master that can starve LTDC fetches?
Are there AXI QoS / arbitration / FIFO states that are:
modified during debug attach
not reset by software reset
not configurable from CubeMX / HAL?
Is there a known erratum or recommended initialization sequence when using LTDC + NPU concurrently?
Is there a way to force a full AXI / interconnect reset or re-arbitration from software?
Are there debug-related side effects (AXI flush, FIFO clear, QoS rebalance) documented somewhere?
Thank you in advance.
Solved! Go to Solution.
2026-03-04 11:57 PM
Hi, I finally find my problem.
When the NPU is running, the majority of exemple of AI project go to sleep mode with __WFE(). But when you do that, some clock might be off if you never configure it. x-cube-ai generate a fonction (with cubeMX) to prevent that : set_clk_sleep_mode.
But you need to add new periph if you enable them in your project, the LTDC for me.
2026-02-24 3:58 AM
I've had the same issue with an audio buffer and frame buffer saved respectively on internal RAM and external PSRAM. Despite accessing it in different times, the images displayed on the LTDC had glitches. At the end of the day, it was both the priority and the speed of access to the external RAM.
Are you using an RTOS? If so, I think you need to tweak the priorities of the threads/tasks.
Also, have you checked the AXIRAM configuration? I would try to speed up the access to it to see if the performances increse
2026-02-24 4:35 AM
No, I'm coding in bare metal.
I will check if I can do something with the AXIRAM config
2026-02-25 1:52 AM
I have enabled LTDC error interrupts and I consistently observe FIFO underrun (FUIF) reported in LTDC ISR2 when the NPU is running in parallel with LTDC.
Key experimental results:
If the AI/NPU is never started, LTDC runs indefinitely without any FUIF or display corruption.
If the AI/NPU runs for a few seconds while LTDC is enabled, a FIFO underrun occurs.
Stopping the AI is NOT sufficient to recover:
The display remains corrupted
FUIF continues to be reported
Only a full LTDC hardware reset via RCC (FORCE_RESET / RELEASE_RESET) restores correct display behavior.
This indicates that a single FIFO underrun permanently corrupts the LTDC internal pipeline/state, and the peripheral does not self-recover.
When I attach a debugger (SWD) once:
LTDC and NPU can run in parallel without any FIFO underrun
No FUIF is ever triggered
The system remains stable even after leaving debug mode and performing software resets
The issue only reappears after a power cycle
If someone have an idea to fix the problem.
Thanks in advance
2026-03-04 11:57 PM
Hi, I finally find my problem.
When the NPU is running, the majority of exemple of AI project go to sleep mode with __WFE(). But when you do that, some clock might be off if you never configure it. x-cube-ai generate a fonction (with cubeMX) to prevent that : set_clk_sleep_mode.
But you need to add new periph if you enable them in your project, the LTDC for me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.