2022-06-24 3:36 PM
I'm new to STM32s and I want to verify that I can put a Quad-SPI PSRAM chip (or SRAM, DRAM, etc) on the Quad-SPI interface and have everything work? From what I have read it seems like it will work, but everything seems to refer to using FLASH memories, not xRAM devices.
The only caveat I see is that the Memory-mapped mode _won't_ work because that is read-only. With that option gone, I'd write some simple code to operate in Indirect Mode (register access) (or perhaps DMA?). My requirements are more storage space than speed. (I need >= 8 Mbits)
So, as I said at the top, I'm just looking for verification that this approach will work.
Thanks!
Solved! Go to Solution.
2022-06-24 4:46 PM
The MCU is relatively agnostic to the type of memory behind the interface. You could use a CPLD/FPGA.
Correct, Memory Mapped doesn't help you, but even for flash, switching back and forth is cumbersome.
2022-06-24 4:46 PM
The MCU is relatively agnostic to the type of memory behind the interface. You could use a CPLD/FPGA.
Correct, Memory Mapped doesn't help you, but even for flash, switching back and forth is cumbersome.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.