2019-05-08 11:11 PM
Hello. I have this init TIM3:
void Start_Timer_3(void)
{
LL_TIM_InitTypeDef TIM_InitStruct;
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_TIM3);
NVIC_SetPriority(TIM3_IRQn, 3);
NVIC_EnableIRQ(TIM3_IRQn);
// 50MHz clock
// 1000 Hz, upcounting 32-bit
// 1000 = ( 50000000 / (Prescaler+1))
TIM_InitStruct.Prescaler = (uint16_t)50000 - 1;
TIM_InitStruct.CounterMode = LL_TIM_COUNTERMODE_UP;
TIM_InitStruct.Autoreload = 0xFFFFFFFFU;
TIM_InitStruct.ClockDivision = LL_TIM_CLOCKDIVISION_DIV1;
TIM_InitStruct.RepetitionCounter = (uint8_t)0x00U;
LL_APB1_GRP1_ForceReset(LL_APB1_GRP1_PERIPH_TIM3);
LL_APB1_GRP1_ReleaseReset(LL_APB1_GRP1_PERIPH_TIM3);
LL_TIM_Init(TIM3, &TIM_InitStruct);
LL_TIM_ClearFlag_UPDATE(TIM3);
LL_TIM_EnableIT_UPDATE(TIM3);
LL_TIM_EnableCounter(TIM3);
}And here is my Handler:
void TIM3_IRQHandler(void)
{
LL_TIM_ClearFlag_UPDATE(TIM3);
// breakpoint atc.... here
}And my handler isn't working. Any idea, why? I try everything.
Solved! Go to Solution.
2019-05-10 3:56 AM
It is my mistake....
Solution is in this line:
TIM_InitStruct.Autoreload = 0xFFFFFFFFU;
2019-05-08 11:49 PM
How do you know that the "handler isn't working"?
Read out the timer registers in debugger, check if they are set as expected, check if TIMx_CNT is changing, check if the required bit in TIMx_UDR is set. Check in NVIC registers if the proper interrupt is enabled. Check in the disassembler if the IRQ handler's address is inserted at the proper place.
I wouldn't be surprised if you'd need to insert some delay between the reset and setting up the timer registers.
JW
2019-05-10 3:56 AM
It is my mistake....
Solution is in this line:
TIM_InitStruct.Autoreload = 0xFFFFFFFFU;
2019-05-15 5:28 AM
I don't understand. What solution? It's exactly as you've posted in your initial post. So what did you do to correct the problem?
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.