2024-10-16 6:01 AM
We are looking into accessing two identical H5 via one SWD connection.
My understanding is that:
- We would need to use third party tools instead of STLink for multi drop support
- The processors support multi drop
- But it does not work with multiple identical processors, because the target identification register (TINSTANCE in DP_DLPIDR) is hardcoded to 0, and cannot be changed.
Is this understanding correct, and if not, what tools would you recommend for multi drop?
Solved! Go to Solution.
2024-10-16 2:23 PM
Dear @KiloMike ,
Your understanding is correct and since the TargetID is the same , the only way is to see the instance ID which we hardcode to 0 at silicon . So not possible to have multi drop chain on SWD with same MCU ID .
https://developer.arm.com/documentation/ddi0314/h/Debug-Access-Port/SW-DP/SW-DP-multi-drop-support
But it should be possible on legacy JTAG serial chain .
STOne-32
2024-10-16 2:23 PM
Dear @KiloMike ,
Your understanding is correct and since the TargetID is the same , the only way is to see the instance ID which we hardcode to 0 at silicon . So not possible to have multi drop chain on SWD with same MCU ID .
https://developer.arm.com/documentation/ddi0314/h/Debug-Access-Port/SW-DP/SW-DP-multi-drop-support
But it should be possible on legacy JTAG serial chain .
STOne-32
2024-10-17 3:40 AM
Thank you for your response
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.