cancel
Showing results for 
Search instead for 
Did you mean: 

Supported PSRAM and Flash for the STM32N6xx

RAdam.1
Associate III
Hey guys,
 
I'm looking for some suitable HexaSPI PSRAM and also the OctoSPI Flash for the STM32N645 board I am just building.. I cant find the parts used on the DK so do you have a list of supported memories? I need 256Mb PSRAM and will start with a 1Gb Flash as per the DK.. 
 
Richard
11 REPLIES 11

We need real-time sensor fusion (data gets streamed in over 5 UARTs and 3 SPI buses) and multiple CNN we would want to switch between to process camera data or sensor data (as a temporal neural network), plus an RGB screen buffer (1024x1024) that needs to update at least 4 times per second. Would splitting the memory into two regions (one for sensor fusion/CNN and one for the screen buffer) be the best approach? Do you think this is feasible?

Hi

I can't reply, let you make calculation of BW versus use case

Alternatively you may use 2 memory on 2 different memory controller

Regards

Alex