STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LTDC Layer1 is only a black box on the STM32N6570-DK

Hello everybody, I am currently trying to get the LTDC running on the STM32N6570-DK without using the HAL drivers.The LTDC itself seems to work partially, because the background color configured via LTDC->BCCR is displayed correctly and can even be c...

Webah by Associate
  • 180 Views
  • 2 replies
  • 0 kudos

Supported PSRAM and Flash for the STM32N6xx

Hey guys, I'm looking for some suitable HexaSPI PSRAM and also the OctoSPI Flash for the STM32N645 board I am just building.. I cant find the parts used on the DK so do you have a list of supported memories? I need 256Mb PSRAM and will start with a 1...

RAdam.1 by Associate III
  • 1311 Views
  • 11 replies
  • 5 kudos

SPI TX DMA Request on Timer Update Event (STM32H7R)

Hello! I'm having issues having a successful configuration for the setup I need: an SPI TX transaction shall occur through DMA once a timer has reached its overflow count. The timer is then reloaded and proceeds to do cyclical SPI TX transactions. I ...

JCori by Associate III
  • 187 Views
  • 4 replies
  • 1 kudos

STM32H723 with SDMMC UHS-I voltage switching

During the initialization of STM32 UHS-I, it has an IO output of 3.3V. After initialization, it outputs at 1.8V. However, I noticed that the external voltage switch transceiver is powered at 1.8V on the host side. I'm afraid it might burn out the ext...

YYT by Associate
  • 236 Views
  • 1 replies
  • 0 kudos

Resolved! Address swapping of SDRAM

Hi ST Community, I am working on STM32H563 with external SDRAM connected through FMC. I am trying to use: heap in SDRAMglobal variables in SDRAMexecution/data access from SDRAMDCACHE enabled Current SDRAM mapping: 0xC0000000 I noticed that in STM32F7...

Resolved! NUCLEO-C562RE boot0 pin issue

Hi, I'm currently developing on the NUCLEO board and I can't enter the bootloader using the boot button on the board. I created an .ioc file with CubeMX2 v1.0.1 using the NUCLEOC562RE board. Then build and flash the code with vscode addon without iss...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.