2017-12-04 4:15 PM
I was wondering if there was any explanation for having several Port E pins (10-13) set to Input (00), and pin E11 is staying high even though there is nothing connected to it. I have tried setting the GPIOE->PUPDR to pull low, but amazingly that does not seem to help. Pin E10 also occasionally toggles without any input.
Here is the relevant code:
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOEEN; // Enable clock for Port E on GPIO
GPIOE->MODER &= ~(0xFF << (2*10)); // Clear bits Pins [10-13] to set to Input (00)Checking the debugger, it appears GPIOE->IDR for pin E11 is constantly a 1, so it doesn't appear to be anything code-related. The only other thing I'm changing on that port is the LED On pin 8.
GPIOE->MODER = ~(3U<<(2*8));
GPIOE->MODER |= 1U<<(2*8); // Output(01) // GPIO Speed: Low speed (00), Medium speed (01), Fast speed (10), High speed (11) GPIOE->OSPEEDR &= ~(3U<<(2*8)); GPIOE->OSPEEDR |= 3U<<(2*8); // High speed // GPIO Output Type: Output push-pull (0, reset), Output open drain (1) GPIOE->OTYPER &= ~(1U<<8); // Push-pull // GPIO Push-Pull: No pull-up, pull-down (00), Pull-up (01), Pull-down (10), Reserved (11) GPIOE->PUPDR &= ~(3U<<(2*8)); // No pull-up, no pull-downHas anyone run into this problem? Colleagues have run into similar problems with other ports like A.
#gpio-port #stm32l476-discovery-board #gpio-alternate-function-ambiguityWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.