STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 BusFault_Handler

Posted on December 05, 2017 at 09:50I'm developing an application based on STM32L4 on a custom board. Program is running fine but I noticed that sometimes (maybe once after four days working) device is reseted. In order to find the reason of this re...

Timer with low power mode

Posted on November 30, 2017 at 11:49Hello all I'm working on STM32L152RE nucleo board. I ain't able to integrate Timer  in low power mode .so is it possible to work with timer and low power mode in STM32L152RE  simultaneously?If yes, which timer is ...

Coin cell to VBAT pin on a Nucleo board?

Posted on November 20, 2017 at 22:35On a Nucleo board, is it as simple as pulling the 0 ohm resistor off SB45, and connecting a coin cell [something like a CR1220] to pin33 [VBAT] and ground, in order to have battery backup for the RTC registers?

Resolved! SD Card using 1 bit SDIO on Nucleo 401Re

Posted on December 02, 2017 at 18:59HI I've been trying to get an SD card working in 1bit mode using the SDIO peripheral. I am failing, and would appreciate some help. I'm on a Nucel401RE using STM32Cube_FW_F4V1.180.0The pin configuration is below. ...

0690X00000604BYQAY.jpg 0690X00000604I8QAI.jpg 0690X00000604HpQAI.jpg 0690X00000604IhQAI.jpg

Resolved! STM32F446RE

Posted on January 20, 2017 at 06:02Hi Guys,I am working on a project based on STM32F446RE and we need to interface external SDRAM(16bit) with STM32. Can anybody help me with interface of SDRAM with STM32.Regards,Muhsin Ali#stm32f446re #sdram

STM32L4 Wakeup Delay from Stop Mode (Stop 0)

Posted on November 27, 2017 at 20:27Question: How to achieve the 4.5 us wakeup time for the stop mode (Stop 0)? The board I am using is STM32L476 NucLeo. I am using the MSI clock (48 MHz) as the system clock. After awaken up, the MCU runs the 'HAL_A...

0690X00000608ySQAQ.png 0690X00000608ycQAA.png

UART IT

Posted on December 04, 2017 at 18:18I am using Nucleo F334 and STM32 Workbench as IDE.I need to build a bridge between UART2 and UART3. It should work this way: data are continously acquired on USART3_RX by interrupt and transmitted on USART2_TX.I a...

Resolved! Firmware Working in Debug but not on Stand Alone

Posted on December 01, 2017 at 16:08Hi,I'm developping a firmware with a stm32f405zgt6Unfortunatly, I debug the code, step by step, and it's working fine, but then, when my board is on stand alone mode, the firmware is not working. It looks it even ...

ignasi by Associate II
  • 2093 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.