2020-07-27 7:15 AM
Hi,
I'm using a STM32L432KC on Windows 10. I installed the ST-LINK driver (009) available on ST website and the ST-LINK utility (004).
When I connect the STM32 to my computer , it doesn't appear as a STM32 device but as follows in 'other devices' of the devices manager:
I installed the STM32CubeIDE and the debug process sends a STLINK error.
The STLINK utility doesn't recognize any STLINK device neither.
How can I solve that properly ?
Thanks
2020-07-27 8:39 AM
Custom board? Do you have an st-link device on the board or are you connecting directly to the chip you want to flash/debug?
2020-07-27 9:14 AM
I have the STM32 nucleo board.
2020-07-27 10:44 AM
>>How can I solve that properly ?
Seems like you have some other stuff installed, that you should probably start by uninstalling.
Check it works on a different computer.
2020-07-27 10:57 AM
I tried on maybe 4 or 5 computers. I installed the ST-link software first then plug the stm32 with usb and this is the only thing appearing in my devices manager.
what am I missing ? A jumper somewhere ?
2020-07-27 12:21 PM
Kind of suggests you've installed different firmware on to the ST-LINK at some point.
2020-07-27 2:26 PM
Is there a way to hard reset it ?
i kind of unpacked it and plugged it and this happened. I don’t what I could have done wrong.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.