STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L432KC is not recognized on my computer

Hi,I'm using a STM32L432KC on Windows 10. I installed the ST-LINK driver (009) available on ST website and the ST-LINK utility (004).When I connect the STM32 to my computer , it doesn't appear as a STM32 device but as follows in 'other devices' of th...

0693W000003BMSuQAO.png
JV1 by Associate II
  • 1943 Views
  • 6 replies
  • 0 kudos

Hi eveyone, i am using stm32f207zg and i want to do a multi channel conversion with adc1. The input pin are PA5 e PA6. The problem is when i play the program: in particulare using debug i note that adc doesn't conversion as the sequence is defined.

int main(void){ double digital; char Stringa[20];   int x=1,k,j,i=0;RCC_CFGR=RCC_CFGR|0xE000;   //clock divided by 16---->APB2 pheripherals CLK = 1MHz RCC_APB1ENR=RCC_APB1ENR|0x20001;    //abilitazione clock per TIMER2 e USART2 RCC_CR=RCC_CR|0x1;   R...

FCa.1 by Associate II
  • 798 Views
  • 0 replies
  • 0 kudos

Discontinuous Mode Tip

It may be obvious to the rest of the world, but in order to get the ADC to operate in Discontinuous Mode, you must also select Scan Mode. This was Not obvious to me from either the comments in the HAL or the reference manual. The SCAN bit in CR1 appa...

Ron Koch by Associate II
  • 1366 Views
  • 0 replies
  • 0 kudos

STM32F7 usart DMA tx

Hello ; I am trying to test usart DMA on F7 . I only can transmite one time ; when i call usart init again its ok . but i still could not understand why . Could you help please while (1) { /* USER CODE END WHILE */   /* USER CODE BE...

Using UART and I2C on the same pins

Hi, I'm using Nucleo-L432KC board and I've got quite a few devices plugged in to it already. And I need to add another device using UART, but I'm using UART2 for debug output already and I2C1 (which always shares pins with UART1) for a couple i2C dev...

kj.obara by Associate III
  • 2276 Views
  • 2 replies
  • 0 kudos

Something wrong in program using STM32F103 ADC.

Dear readerI hope someone can help me with my question. I have programmed an ADC1 on a STM32F103 with the following functions activated:Continues conversion modeScan mode with two channels A0 And A1 DMA to an array in memory ADC_data[2]( ADC Interrup...

WOGoos by Associate II
  • 2001 Views
  • 4 replies
  • 0 kudos

STM32G474 - using upper 16kB of CCM-SRAM breaks debugging

Hi guys, I have a crazy curiosity at my hands. The STM32G474 is a "category 3" device, therefore it has 128kB of RAM with the upper 32kB being CCM-SRAM. It is really nice that it is all addressable in one continuous block.When i use the upper 16kB of...

Albi G. by Senior
  • 1444 Views
  • 0 replies
  • 0 kudos

Resolved! Example for using DAC on STM32

Hello,I'm working with the NUCLEO-F722ZE EVB on STM32CubeIDE.I'm Looking for a C example that explains how to use the device's DAC (Digital to Analog Converter)

skon.1 by Senior
  • 1941 Views
  • 2 replies
  • 0 kudos

Why (stm32 discovery) pins are resetting ?

When i use iar embeded workbench its work correctly with out f11 .While it works by itself , its pins are resetting.I want to learn what happening here .Even power is enough.Model : stm32f429COD:CONTROLREAD LDR R0, =USART2_DR         LDR R1, [R...

YAY.1 by Senior
  • 6137 Views
  • 14 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.