2020-07-27 9:46 AM
Hi,
I am using stm32431. I config LPTIM and call HAL_LPTIM_Counter_Start() but return HAL_TIMEOUT and no pulses is count. When I change HAL_LPTIM_Counter_Start() function putting 'HAL_OK' to be return forced, the pulses is counted normally, but not in every time, some yes some no.
The function that i changed:
if (LPTIM_WaitForFlag(hlptim, LPTIM_FLAG_ARROK) == HAL_TIMEOUT)
{
// return HAL_TIMEOUT;
return HAL_OK;
}
Why is returned HAL_TIMEOUT ?
P.S I know that need 5 pulses to begin count.
2020-07-27 9:50 AM
as a matter of fac, I comment "if (LPTIM_WaitForFlag(hlptim, LPTIM_FLAG_ARROK) == HAL_TIMEOUT)", not put return OK as I said, so the waitforflag is ignored.
2020-07-27 10:37 AM
Use a debugger to inspect timer registers. Check register values with reference manual to verify correct bits are set
2020-07-27 10:43 AM
On STM32L4R I use LPTIM to drive buzzer audio notes or short delays in used. Code extract: (48MHz SYSCLK)
Maybe you'll find some clues from this?
extern LPTIM_HandleTypeDef hlptim1;
void LPTIM1_Init(void) {
LPTIM_HandleTypeDef* hlptim = &hlptim1;
// Set the LPTIM2 clock to PCLK because HSI16 is off
// RCC->CCIPR &= ~(3<<20);
// RCC->CCIPR |= (0<<20); 48 MHz = MSI = APB
HAL_NVIC_SetPriority(LPTIM1_IRQn, 2/*0*/, 0);
HAL_NVIC_EnableIRQ(LPTIM1_IRQn);
hlptim->Instance->CFGR |= LPTIM_PRESCALER_DIV16; // 3 ticks = 1 us
/* Set WAVE bit to enable the set once mode */
hlptim->Instance->CFGR |= LPTIM_CFGR_PRELOAD;// LPTIM_CFGR_WAVE;
/* Enable Autoreload match interrupt */
hlptim->Instance->ICR |= 0x0002; // ARRMCF clear flag
__HAL_LPTIM_ENABLE_IT(hlptim, LPTIM_IT_ARRM);
/* Enable Compare match interrupt */
// __HAL_LPTIM_ENABLE_IT(hlptim, LPTIM_IT_CMPM);
/* Enable the Peripheral */
// __HAL_LPTIM_ENABLE(hlptim);
}
void LPTIM1_SetTick_us(uint32_t delay_us) {
LPTIM_HandleTypeDef* hlptim = &hlptim1;
if((delay_us/3)>0xFFFF) TrapError(); // change the clock prescaler if looking at more than one milisecond
if(delay_us==0) {
// turn the timer event off
__HAL_LPTIM_DISABLE_IT(hlptim, LPTIM_IT_ARRM);
__HAL_LPTIM_DISABLE(hlptim);
return; // done
}
/* Enable Autoreload match interrupt */
__HAL_LPTIM_ENABLE_IT(hlptim, LPTIM_IT_ARRM);
/* Enable Compare match interrupt */
// __HAL_LPTIM_ENABLE_IT(hlptim, LPTIM_IT_CMPM);
/* Enable the Peripheral */
__HAL_LPTIM_ENABLE(hlptim);
/* Load the period value in the autoreload register */
__HAL_LPTIM_AUTORELOAD_SET(hlptim, delay_us * 3);
/* Start timer in freerun mode */
__HAL_LPTIM_START_CONTINUOUS(hlptim);
}
void LPTIM1_SetPWM_us(uint32_t delay_us) { // this delay is the half period
LPTIM_HandleTypeDef* hlptim = &hlptim1;
if((delay_us/3)>0xFFFF) TrapError(); // change the clock prescaler if looking at more than one milisecond
if(delay_us==0) {
// turn the timer event off
__HAL_LPTIM_DISABLE_IT(hlptim, LPTIM_IT_ARRM);
__HAL_LPTIM_DISABLE(hlptim);
return; // done
}
/*HAL_StatusTypeDef*/ HAL_LPTIM_PWM_Start(hlptim, delay_us * 3 * 2, delay_us * 3);
return;
__HAL_LPTIM_COMPARE_SET(hlptim, delay_us * 3);
/* Enable Autoreload match interrupt */
//- __HAL_LPTIM_ENABLE_IT(hlptim, LPTIM_IT_ARRM);
__HAL_LPTIM_DISABLE_IT(hlptim, LPTIM_IT_ARRM);
/* Enable Compare match interrupt */
// __HAL_LPTIM_ENABLE_IT(hlptim, LPTIM_IT_CMPM);
/* Enable the Peripheral */
__HAL_LPTIM_ENABLE(hlptim);
/* Load the period value in the autoreload register */
__HAL_LPTIM_AUTORELOAD_SET(hlptim, delay_us * 3 * 2); // it becomes the period
/* Start timer in freerun mode */
__HAL_LPTIM_START_CONTINUOUS(hlptim);
}
/*
void HAL_LPTIM_AutoReloadMatchCallback(LPTIM_HandleTypeDef *hlptim) {
// Timer is one shot mode, so it should trigger only once after kitstarted
NOPs(1);
}
*/
void LPTIM1_IRQHandler(void) {
// HAL_LPTIM_IRQHandler(&hlptim1); // ==> HAL_LPTIM_AutoReloadMatchCallback(&hlptim2);
/* Autoreload match interrupt */
if(__HAL_LPTIM_GET_FLAG(&hlptim1, LPTIM_FLAG_ARRM) != RESET)
{
if(__HAL_LPTIM_GET_IT_SOURCE(&hlptim1, LPTIM_IT_ARRM) != RESET)
{
/* Clear Autoreload match flag */
__HAL_LPTIM_CLEAR_FLAG(&hlptim1, LPTIM_FLAG_ARRM);
/* Autoreload match Callback */
...
}
}
}
2020-07-27 2:40 PM
What is the LPTIM clock?
JW
2020-07-27 3:19 PM
Thank you !!!!
2020-07-27 3:21 PM
I tried, LSE, HSE, HSI. The same timeout. The problem is in 'LPTIM_FLAG_ARROK' I think.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.