2018-03-13 3:04 PM
Hello,
DS12110 rev. 3 in table 51 .' Flash memory programming (single bank configuration nDBANK=1)' misses values for sector erase time with parallelisme x32 and misses even an entry for parallesim x64.
2018-03-16 9:18 AM
Hello
Bonnes.Uwe
,You are right, there is a missing values for '
sector (128 KB) erase time':
- Program/erase parallelism x 32 :
typ = 1,1 and max = 2,2
-Program/erase parallelism x 64 :
typ = 1 and max = 2
The missing values will be added
in next release of H7 datasheets.
Best Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.