2019-03-22 11:36 AM
Hello,
Due to so attractive price + some specific features, the H7 Value Line looks to me very attractive to take into a new design, but 128kB Flash is not enough for me, I have to take an external flash, which is QSPI. I have a few basic questions about that.
1. I am almost sure that Quad-SPI works with the Value line H7 as well, but since I saw in some doc that an H7 Discovery works with Dual SPI only, I have some hesitation. Can one here confirm that?
2. If work through Quad-SPI (QSPI Memory Mapped), how the performance will be reduced vs a normal mode @ 400MHz?
3. Does this Quad-SPI make debugging more complicated? What issues did you face , especially with Atollic?
4. Does ST-Link support H7 programming with Quad-SPI enabled?
5. What are other issues with H7 + Quad SPI, you would recommend me to take in account ?
Thanks!
2019-03-31 12:41 PM
Thank you Andreas for the answer.
"If the benchmark spends most of the time in tight loops, cache is enabled, "
I don't think the real life code looks like you described above.
Anyways, there is 1MB RAM and I don't think I need more than let's say 50K, so do you agree that running from internal SRAM is a better alternative than XIP, 2 X QPI, because :
Your help is very valuable, appreciate that!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.